Other Parts Discussed in Thread: OMAP3525
We're using the OMAP3525 (and developing at the moment with the OMAP35x EVM).
1. What’s the difference between OMAP2430 MMC/SD/SDIO and OMAP3525 MMC/SD/SDIO? Are they register compatible? If not, are there substantial functional differences? We're preparing to integrate a WiFi/Bluetooth module that is supposedly functional with the 2430.
2. Can anyone confirm for me that each MMC/SD/SDIO interface can only support a single device? If so, is this a limitation of the OMAP or a restriction of the MMC/SD/SDIO specifications/interface?
3. I haven’t looked closely at all the GPIO mux’ing options, but can anyone tell me if using MMC3 (in addition to MMC1 and MMC2) precludes any other OMAP3525 functionality?
Thanks.