This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

L3 interconnect backtrace

I am getting the following kernel crash continuously after linux got booted up. What could be the possibility of getting this  l3 debug or l3 application interrupts?

[   36.728210] WARNING: at drivers/bus/omap_l3_noc.c:113 l3_interrupt_handler+0xbc/0x158()
[   36.728607] L3 custom error: MASTER:MPU TARGET:GPMC
[   36.729095] [<c001a898>] (unwind_backtrace+0x0/0xf8) from [<c00439f8>] (warn_slowpath_common+0x4c/0x64)
[   36.729583] [<c00439f8>] (warn_slowpath_common+0x4c/0x64) from [<c0043aa4>] (warn_slowpath_fmt+0x30/0x40)
[   36.730041] [<c0043aa4>] (warn_slowpath_fmt+0x30/0x40) from [<c02beaf0>] (l3_interrupt_handler+0xbc/0x158)
[   36.730529] [<c02beaf0>] (l3_interrupt_[   36.860809] [<c001a898>] (unwind_backtrace+0x0/0xf8) from [<c00439f8>] )
[   36.861297] [<c00439f8>] (warn_slowpath_common+0x4c/0x64) from [<c0043aa4>] (warn_slowpath_fmt+0x30/0x40)
[   36.861755] [<c0043aa4>] (warn_slowpath_fmt+0x30/0x40) from [<c02beaf0>] (l3_interrupt_handler+0xbc/0x158)
[   36.862243] [<c02beaf0>] (l3_interrupt_handler+0xbc/0x158) from [<c00a1ed8>] (handle_irq_event_percpu+0x5c/0x25c)
[   36.862762] [<c00a1ed8>] (handle_irq_event_percpu+0x5c/0x25c) from [<c00a2114>] (handle_irq_event+0x3c/0x5c)
[   36.863250] [<c00a2114>] (handle_irq_event+0x3c/0x5c) from [<c00a4cd4>] (handle_fasteoi_irq+0x7c/0x138)
[   36.863739] [<c00a4cd4>] (handle_fasteoi_irq+0x7c/0x138) from [<c00a18b8>] (generic_handle_irq+0x20/0x30)
[   36.864196] [<c00a18b8>] (generic_handle_irq+0x20/0x30) from [<c0013f14>] (handle_IRQ+0x38/0x90)
[   36.864654] [<c0013f14>] (handle_IRQ+0x38/0x90) from [<c000850c>] (gic_handle_irq+0x28/0x5c)
[   36.865081] [<c000850c>] (gic_handle_irq+0x28/0x5c) from [<c054ef04>] (__irq_svc+0x44/0x58)
[   36.865478] Exception stack(0xc0ecff58 to 0xc0ecffa0)
[   36.865753] ff40:                                                       c001417c c0ed6ac0
[   36.866149] ff60: 00000000 c002ff28 c0ece000 c0ece000 c0f92f08 c055a95c c0edadd0 412fc0f2
[   36.866577] ff80: c0ece000 00000000 60000013 c0ecffa0 c001417c c0014180 60000013 ffffffff
[   36.866973] [<c054ef04>] (__irq_svc+0x44/0x58) from [<c0014180>] (default_idle+0x20/0x30)
[   36.867401] [<c0014180>] (default_idle+0x20/0x30) from [<c00142dc>] (cpu_idle+0x50/0x104)
[   36.867797] [<[