Hi,
I would like to use the System Analyzer in the EtherCAT full application, but nothing is display when entering the Live Sessions.
I added the UIA and the LoggingSetup to the SYSBIOS *.cfg-File, but as I said nothing is displayed. If I use the same UIA and Logging configuration to the uartecho *.cfg it works perfectly.
What am I doing wrong? Is there something I have to enable to get tey System Anlayzer support in ecat_appl project?
Regards,
Klaus
CCS 5.5.0.00077 ; XDC Tools 3.25.3.72 ; SYSBIOS 6.35.4.50 ; UIA 1.3.1.08