Other Parts Discussed in Thread: DM8107, TVP5158
Hello All,
I am working on integrating TW2867 Decoder chip on DM8107 SOC.Mentioning the details below.
1) I have configured TW2867 Decoder in the dvr_rdk/mcfw/src_linux/devices/
2) Currently using USECASE : dvr_rdk/mcfw/src_linux//mcfw_api/usecases/multiprogrssive_4d1_xxxx
OBSERVATIONS :
1) TW2867 detects Video and also detects Video Standard(PAL/MNTSC) of the analog video camera .
2) Display shows vertical lines of dark and white pattern alternatively. When Camera is connected.
3)In HDVPSS,Capture Module get the data and following functions are called.
# CaptureLink_drvCallBack -> CaptureLink_drvProcessData
# CaptureLink_drvProcessData -> Deque Frames for all Active Handles
#But this func ,not able to ASSERT FVID2 Capture Driver and also System_sendLinkCmd() doesn't get invoked.
#CaptureLink_drvOverflowDetectAndReset() function gets invoked ,but no Display overflow detected.
LOGS: I am attaching the logs of capture advanced stats .
Note: As observed in TVP5158 , CaptureLink_drvProcessData asserts FVID2 Capture Driver and send data available messages to next task.
Please suggest me over this issue.What steps i have to take further?
Regards
Nitish Mehta
BELOW ARE THE LOGS :
########################################################################################
NOTE : Please note that 2968/2867 showing strings on logs belongs to 2867 only.
********* Entered usecase 4CH <8107> Enc/Dec OSD Disabled SCD Enabled
149: MCFW : CPU Revision [ES1.0] !!!
DEVICE: TW2968: Chip ID: 0xfe=0x00, 0xff=0xc8!!!
VCAP: DEVICE-0 (0x28): Chip ID 0x0019, Rev 0x0000, Firmware 0x0000 !!!
DEVICE: TW2968: Video Status: 0x00=0x69,CHIP STATUS:0x0d=0x10,STD_SEL: 0x0e=0x17 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
TW2968: Video Is Detected
VCAP: DEVICE-0 (0x28): Detected video (720x288@50Hz, 1) !!!
DEVICE: TW2968: CH0: HACTIVE (720): 0x07=0x12, 0x0b=0xd0!!!
DEVICE: TW2968: CH0: VDELAY (18): 0x08=0x12, 0x09=0x20!!!
DEVICE: TW2968: CH1: HACTIVE (720): 0x17=0x12, 0x1b=0xd0!!!
DEVICE: TW2968: CH1: VDELAY (18): 0x18=0x12, 0x19=0x20!!!
DEVICE: TW2968: CH2: HACTIVE (720): 0x27=0x12, 0x2b=0xd0!!!
DEVICE: TW2968: CH2: VDELAY (18): 0x28=0x12, 0x29=0x20!!!
DEVICE: TW2968: CH3: HACTIVE (720): 0x37=0x12, 0x3b=0xd0!!!
DEVICE: TW2968: CH3: VDELAY (18): 0x38=0x12, 0x39=0x20!!!
DEVICE: TW2968: Set Video Mode Done !!!
[m3vpss ] 5021: CAPTURE: Create in progress !!!
[m3vpss ] CAPTURE: CaptureLink_drvCallback
[m3vpss ] CAPTURE: CaptureLink_drvCallback
[m3vpss ] CAPTURE: CaptureLink_drvCallback
[m3vpss ] CAPTURE: CaptureLink_drvCallback
[m3vpss ] CAPTURE: CaptureLink_drvCallback
[m3vpss ] CAPTURE: CaptureLink_drvCallback
[m3vpss ] 5032: CAPTURE: VIP0 PortA capture mode is [ 8-bit, Pixel-mux Embedded Sync] !!!
[m3vpss ] CAPTURE:Create args numBufsPerCh[5] < min[6]Overriding create args
[m3vpss ] UTILS: DMA: Allocated CH (TCC) = 58 (58)
[m3vpss ] UTILS: DMA: 0 of 4: Allocated PaRAM = 58 (0x49004740)
[m3vpss ] UTILS: DMA: 1 of 4: Allocated PaRAM = 64 (0x49004800)
[m3vpss ] UTILS: DMA: 2 of 4: Allocated PaRAM = 65 (0x49004820)
[m3vpss ] UTILS: DMA: 3 of 4: Allocated PaRAM = 66 (0x49004840)
[m3vpss ] CAPTURE::HEAPID:0 USED:328
[m3vpss ] CAPTURE::HEAPID:4 USED:10174464
[m3vpss ] 5089: CAPTURE: Create Done !!!
[m3vpss ] 5089: NSF: Create in progress !!!
[m3vpss ] NSF::HEAPID:0 USED:128
[m3vpss ] NSF::HEAPID:1 USED:9152
[m3vpss ] NSF::HEAPID:4 USED:6082560
[m3vpss ] 5124: NSF: Create Done !!!
[m3vpss ] 5124: DEI : Create in progress !!!
[m3vpss ] 5214: DEI : Loading Up-scaling Co-effs
[m3vpss ] 5214: DEI : Co-effs Loading ... DONE !!!
[m3video] 5239: IPC_IN_M3 : Create in progress !!!
[m3vpss ] DEI:HEAPID:0 USED:64
[m3video] 5239: SYSTEM: Opening ListMP [VPSS-M3_IPC_OUT_0] ...
[m3vpss ] DEI:HEAPID:1 USED:9600
[m3video] 5239: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_0] ...
[m3vpss ] DEI:HEAPID:4 USED:15611904
[m3vpss ] 5215: DEI : Create Done !!!
[m3vpss ] 5220: DUP : Create Done !!!
[m3vpss ] 5221: NSF: Create in progress !!!
[m3video] 5242: IPC_IN_M3 : Create Done !!!
[m3video] 5243: ALG : Create in progress !!!
[m3vpss ] NSF::HEAPID:0 USED:128
[m3vpss ] NSF::HEAPID:1 USED:5632
[m3vpss ] NSF::HEAPID:4 USED:2433024
[m3vpss ] 5235: NSF: Create Done !!!
[m3vpss ] 5237: MERGE : Create Done !!!
[m3vpss ] 5237: IPC_OUT_M3 : Create in progress !!!
[m3vpss ] 5238: IPC_OUT_M3 : Create Done !!!
[m3video] 5255: ALG : Prev Link ID = 10000002 !!!
[m3video] 5255: SCD: Opening algorithm ... !!!
[m3video] 5256: SCD: Opening algorithm ... DONE !!!
[host] 418: IPC_BITS_OUT : Create in progress !!!
[host] IPC_BITSOUT:BitBuffer Alloc.ChID:0,Size:0x25F800
[host]
******* RingBuf 0 created ********
[host] IPCBITSOUTLINK:Translated Addr Virt:0x41d82080 To Phy:0x95000080
[host]
###Bit buff of size from the SR # 1 : 2488320 / bufsize 414720, maxQueueDepth 50
[host] ###Bit buff BasePtr: 41D82080 / PhyAddr 95000080
[host] IPC_BITSOUT:BitBuffer Alloc.ChID:1,Size:0x25F800
[host]
******* RingBuf 1 created ********
[host] IPCBITSOUTLINK:Translated Addr Virt:0x41fe1880 To Phy:0x9525f880
[host]
###Bit buff of size from the SR # 1 : 2488320 / bufsize 414720, maxQueueDepth 50
[host] ###Bit buff BasePtr: 41FE1880 / PhyAddr 9525F880
[host] IPC_BITSOUT:BitBuffer Alloc.ChID:2,Size:0x25F800
[host]
******* RingBuf 2 created ********
[host] IPCBITSOUTLINK:Translated Addr Virt:0x42241080 To Phy:0x954bf080
[host]
###Bit buff of size from the SR # 1 : 2488320 / bufsize 414720, maxQueueDepth 50
[host] ###Bit buff BasePtr: 42241080 / PhyAddr 954BF080
[host] IPC_BITSOUT:BitBuffer Alloc.ChID:3,Size:0x25F800
[host]
******* RingBuf 3 created ********
[host] IPCBITSOUTLINK:Translated Addr Virt:0x424a0880 To Phy:0x9571e880
[host]
###Bit buff of size from the SR # 1 : 2488320 / bufsize 414720, maxQueueDepth 50
[host] ###Bit buff BasePtr: 424A0880 / PhyAddr 9571E880
[host] 420: IPC_BITS_OUT : Create Done !!!
[m3video] UTILS: DMA: Allocated CH (TCC) = 50 (50)
[m3video] UTILS: DMA: 0 of 1: Allocated PaRAM = 50 (0x49004640)
[m3video] ALGLINK:HEAPID:0 USED:14336
[m3video] ALGLINK:HEAPID:3 USED:3425408
[m3video] 5275: ALG : Create Done !!!
[m3video] 5279: IPC_BITS_IN : Create in progress !!!
[m3video] 5280: SYSTEM: Opening ListMP [HOST_IPC_OUT_24] ...
[m3video] 5280: SYSTEM: Opening ListMP [HOST_IPC_IN_24] ...
[m3video] 5281: SYSTEM: Opening MsgQ [HOST_MSGQ] ...
[m3video] 5283: IPC_BITS_IN : Create Done !!!
[m3video] 5283: DECODE: Create in progress ... !!!
[m3video] DECLINK_H264:HEAPID:0 USED:4264
[m3video] DECLINK_H264:HEAPID:3 USED:1433600
[m3video] 5297: DECODE: Creating CH0 of 720 x 576 [PROGRESSIVE] [TILED ],target bitrate = 2000 Kbps ...
[m3video] DECLINK_H264:HEAPID:0 USED:2368
[m3video] DECLINK_H264:HEAPID:3 USED:1433600
[m3video] 5309: DECODE: Creating CH1 of 720 x 576 [PROGRESSIVE] [TILED ],target bitrate = 2000 Kbps ...
[m3video] DECLINK_H264:HEAPID:0 USED:2368
[m3video] DECLINK_H264:HEAPID:3 USED:1433600
[m3video] 5322: DECODE: Creating CH2 of 720 x 576 [PROGRESSIVE] [TILED ],target bitrate = 2000 Kbps ...
[m3video] DECLINK_H264:HEAPID:0 USED:2368
[m3video] DECLINK_H264:HEAPID:3 USED:1433600
[m3video] 5335: DECODE: Creating CH3 of 720 x 576 [PROGRESSIVE] [TILED ],target bitrate = 2000 Kbps ...
[m3video] 5337: DECODE: All CH Create ... DONE !!!
[m3video] DECLINK:HEAPID:0 USED:11408
[m3video] DECLINK:HEAPID:3 USED:5734400
[m3video] 5339: DECODE: Create ... DONE !!!
[m3video] 5339: ENCODE: Create in progress ... !!!
[m3video] ENCLINK:INFO: !!!Number of output buffers for ch[8] set to [1]
[m3video] 5373: ENCODE: Creating CH0 of 704 x 576, pitch = (16384, 32768) [PROGRESSIVE] [TILED ], bitrate = 2000 Kbps ...
[host] IpcBitsInLink_tskMain:Entered
[host] 556: IPC_BITS_IN : Create in progress !!!
[host] 556: IPC_BITS_IN : ListMPOpen start !!!
[host] 556: SYSTEM: Opening ListMP [VIDEO-M3_IPC_OUT_24] ...
557: SYSTEM: Opening ListMP [VIDEO-M3_IPC_IN_24] ...
[host] 559: IPC_BITS_IN : ListMPOpen done !!!
[host] 560: IPC_BITS_IN : System_linkGetInfo done !!!
[host] 560: IPC_BITS_IN : Create Done !!!
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3vpss ] 5421: IPC_IN_M3 : Create in progress !!!
[m3video] ENCLINK_H264:HEAPID:3 USED:49152
[m3vpss ] 5421: SYSTEM: Opening ListMP [VIDEO-M3_IPC_OUT_0] ...
[m3video] 5377: ENCODE: Creating CH1 of 704 x 576, pitch = (16384, 32768) [PROGRESSIVE] [TILED ], bitrate = 2000 Kbps ...
[m3vpss ] 5422: SYSTEM: Opening ListMP [VIDEO-M3_IPC_IN_0] ...
[m3vpss ] 5422: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3vpss ] 5425: IPC_IN_M3 : Create Done !!!
[m3video] ENCLINK_H264:HEAPID:3 USED:49152
[m3vpss ] 5426: MERGE : Create Done !!!
[m3video] 5381: ENCODE: Creating CH2 of 704 x 576, pitch = (16384, 32768) [PROGRESSIVE] [TILED ], bitrate = 2000 Kbps ...
[m3vpss ] 5431: DUP : Create Done !!!
[m3vpss ] 5432: SWMS: Create in progress !!!
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3video] ENCLINK_H264:HEAPID:3 USED:49152
[m3video] 5385: ENCODE: Creating CH3 of 704 x 576, pitch = (16384, 32768) [PROGRESSIVE] [TILED ], bitrate = 2000 Kbps ...
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3video] ENCLINK_H264:HEAPID:3 USED:49152
[m3video] 5390: ENCODE: Creating CH4 of 352 x 288, pitch = (352, 352) [PROGRESSIVE] [NON-TILED ], bitrate = 500 Kbps ...
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3video] ENCLINK_H264:HEAPID:3 USED:577536
[m3video] 5394: ENCODE: Creating CH5 of 352 x 288, pitch = (352, 352) [PROGRESSIVE] [NON-TILED ], bitrate = 500 Kbps ...
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3video] ENCLINK_H264:HEAPID:3 USED:577536
[m3video] 5399: ENCODE: Creating CH6 of 352 x 288, pitch = (352, 352) [PROGRESSIVE] [NON-TILED ], bitrate = 500 Kbps ...
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3video] ENCLINK_H264:HEAPID:3 USED:577536
[m3video] 5404: ENCODE: Creating CH7 of 352 x 288, pitch = (352, 352) [PROGRESSIVE] [NON-TILED ], bitrate = 500 Kbps ...
[m3video] ENCLINK_H264:HEAPID:0 USED:11912
[m3video] ENCLINK_H264:HEAPID:3 USED:577536
[m3video] 5409: ENCODE: Creating CH8 of 704 x 576, pitch = (704, 704) [PROGRESSIVE] [NON-TILED ], bitrate = 100 Kbps ...
[m3vpss ] UTILS: DMA: Allocated CH (TCC) = 59 (59)
[m3video] ENCLINK_JPEG:HEAPID:0 USED:2064
[m3vpss ] UTILS: DMA: 0 of 1: Allocated PaRAM = 59 (0x49004760)
[m3video] 5409: ENCODE: Creating CH9 of 704 x 576, pitch = (704, 704) [PROGRESSIVE] [NON-TILED ], bitrate = 100 Kbps ...
[m3vpss ] SWMS: instance 0, sc id 4, start win 0 end win 17
[m3vpss ] AVSYNC:WARNING!! Application wrongly configureddisplayID[-1]. Reseting to correct displayID[0]
[m3video] ENCLINK_JPEG:HEAPID:0 USED:2064
[m3vpss ] WARNING: WIN0: CH8, Channel ID is INVALID (max allowed CH ID is CH7), !!!
[m3video] 5410: ENCODE: Creating CH10 of 704 x 576, pitch = (704, 704) [PROGRESSIVE] [NON-TILED ], bitrate = 100 Kbps ...
[m3vpss ] SWMS:HEAPID:0 USED:224
[m3video] ENCLINK_JPEG:HEAPID:0 USED:2064
[m3vpss ] SWMS:HEAPID:1 USED:47296
[m3video] 5411: ENCODE: Creating CH11 of 704 x 576, pitch = (704, 704) [PROGRESSIVE] [NON-TILED ], bitrate = 100 Kbps ...
[m3vpss ] SWMS:HEAPID:3 USED:4147200
[m3vpss ] SWMS:HEAPID:4 USED:16588800
[m3vpss ] 5555: SWMS: Create Done !!!
[m3video] ENCLINK_JPEG:HEAPID:0 USED:2064
[m3vpss ] 5555: SWMS: Create in progress !!!
[m3video] 5412: ENCODE: All CH Create ... DONE !!!
[m3vpss ] UTILS: DMA: Allocated CH (TCC) = 60 (60)
[m3vpss ] UTILS: DMA: 0 of 1: Allocated PaRAM = 60 (0x49004780)
[m3vpss ] SWMS: instance 0, sc id 5, start win 0 end win 17
[m3video] ENCLINK:HEAPID:0 USED:103592
[m3video] ENCLINK:HEAPID:2 USED:5676800
[m3vpss ] AVSYNC:WARNING!! Application wrongly configureddisplayID[-1]. Reseting to correct displayID[1]
[m3video] ENCLINK:HEAPID:3 USED:2506752
[m3video] 5412: ENCODE: Create ... DONE !!!
[m3video] 5413: IPC_BITS_OUT : Create in progress !!!
[m3vpss ] SWMS:HEAPID:0 USED:224
[m3vpss ] SWMS:HEAPID:1 USED:47296
[m3vpss ] SWMS:HEAPID:3 USED:2543616
[m3video] 5415: IPC_BITS_OUT : Create Done !!!
[m3vpss ] SWMS:HEAPID:4 USED:3391488
[m3video] 5420: IPC_OUT_M3 : Create in progress !!!
[m3vpss ] 5599: SWMS: Create Done !!!
[m3video] 5421: IPC_OUT_M3 : Create Done !!!
[m3vpss ] 5599: DISPLAY: Create in progress !!!
[m3vpss ] 5600: DISPLAY: Create Done !!!
[m3vpss ] 5601: DISPLAY: Create in progress !!!
[m3vpss ] 5601: DISPLAY: 43: Field Separate Mode ENABLED for Que 0 !!!
[m3vpss ] 5602: DISPLAY: Create Done !!!
24/01/2000 09:54:01
SYS_LOG : D : checkLinkStatusCB[681] : Lan 01 is UP now
Close Channel: 0
IPCBITS Close Channel: 0
[host]
2017: IPCBITSOUT:Link[30000018]:
[host] Flush Frame Sent for chId[0] [m3video] DEC : Delete CH0 Got the Dummy Object queued !!!
[m3video] 6870: DECODE: CH0: Decoder flush needed (0)!!!
[m3video] 6870: DECODE: CH0: Decoder Flushing !!!
[m3video] DEC : Delete CH0, Dummy Object queued !!!
[m3video] MemoryLeak:STAGE:0 HEAPNUM:0 ALLOC=4264 FREED=2368
[host]
2039: IPCBITSOUT:Link[30000018]:
[host] Flush Frame Received for chId[0]
[host] IPC_BITSOUT:BitBuffer Free.chID:0,Size:0x25F800
[host] ******* RingBuf 0 deleted ********
[host]
2041: IPCBITSOUT:Link[30000018]:
[host] Ch buffer delete completed for chId[0].Total Time[24] [m3video] 6882: IPCBITSIN:Link[1000001a]:
[m3video] Flush Frame received for ch[0]
[m3video] 6882: DECODE: CH0:
[m3video] Queing flush Frame to processQ
[m3video] 6882: DECODE: CH0:
[m3video] Flush Frame Received in ProcessQue
[m3video] 6886: DECODE: CH0:
[m3video] Freeing flush Frame
[m3video] 6886: IPCBITSIN:Link[1000001a]:
[m3video] Flush Frame freed for ch[0]
Close Channel: 1
IPCBITS Close Channel: 1
[host]
2049: IPCBITSOUT:Link[30000018]:
[host] Flush Frame Sent for chId[1] [m3video] DEC : Delete CH1 Got the Dummy Object queued !!!
[m3video] 6901: DECODE: CH1: Decoder flush needed (0)!!!
[m3video] 6902: DECODE: CH1: Decoder Flushing !!!
[m3video] DEC : Delete CH1, Dummy Object queued !!!
[host]
2071: IPCBITSOUT:Link[30000018]:
[host] Flush Frame Received for chId[1]
[host] IPC_BITSOUT:BitBuffer Free.chID:1,Size:0x25F800
[host] ******* RingBuf 1 deleted ********
[host]
2073: IPCBITSOUT:Link[30000018]:
[host] Ch buffer delete completed for chId[1].Total Time[24] [m3video] 6914: IPCBITSIN:Link[1000001a]:
[m3video] Flush Frame received for ch[1]
[m3video] 6914: DECODE: CH1:
[m3video] Queing flush Frame to processQ
[m3video] 6914: DECODE: CH1:
[m3video] Flush Frame Received in ProcessQue
[m3video] 6918: DECODE: CH1:
[m3video] Freeing flush Frame
[m3video] 6918: IPCBITSIN:Link[1000001a]:
[m3video] Flush Frame freed for ch[1]
Close Channel: 2
IPCBITS Close Channel: 2
[host]
2080: IPCBITSOUT:Link[30000018]:
[host] Flush Frame Sent for chId[2] [m3video] DEC : Delete CH2 Got the Dummy Object queued !!!
[m3video] 6933: DECODE: CH2: Decoder flush needed (0)!!!
[m3video] 6934: DECODE: CH2: Decoder Flushing !!!
[m3video] DEC : Delete CH2, Dummy Object queued !!!
[host]
2103: IPCBITSOUT:Link[30000018]:
[host] Flush Frame Received for chId[2]
[host] IPC_BITSOUT:BitBuffer Free.chID:2,Size:0x25F800
[host] ******* RingBuf 2 deleted ********
[host]
2105: IPCBITSOUT:Link[30000018]:
[host] Ch buffer delete completed for chId[2].Total Time[25] [m3video] 6946: IPCBITSIN:Link[1000001a]:
[m3video] Flush Frame received for ch[2]
[m3video] 6946: DECODE: CH2:
[m3video] Queing flush Frame to processQ
[m3video] 6946: DECODE: CH2:
[m3video] Flush Frame Received in ProcessQue
[m3video] 6950: DECODE: CH2:
[m3video] Freeing flush Frame
[m3video] 6950: IPCBITSIN:Link[1000001a]:
[m3video] Flush Frame freed for ch[2]
Close Channel: 3
IPCBITS Close Channel: 3
[host]
2112: IPCBITSOUT:Link[30000018]:
[host] Flush Frame Sent for chId[3] [m3video] DEC : Delete CH3 Got the Dummy Object queued !!!
[m3video] 6965: DECODE: CH3: Decoder flush needed (0)!!!
[m3video] 6965: DECODE: CH3: Decoder Flushing !!!
[m3video] DEC : Delete CH3, Dummy Object queued !!!
[host]
2135: IPCBITSOUT:Link[30000018]:
[host] Flush Frame Received for chId[3]
[host] IPC_BITSOUT:BitBuffer Free.chID:3,Size:0x25F800
[host] ******* RingBuf 3 deleted ********
[host]
2137: IPCBITSOUT:Link[30000018]:
[host] Ch buffer delete completed for chId[3].Total Time[25] [m3video] 6978: IPCBITSIN:Link[1000001a]:
[m3video] Flush Frame received for ch[3]
[m3video] 6978: DECODE: CH3:
[m3video] Queing flush Frame to processQ
[m3video] 6978: DECODE: CH3:
[m3video] Flush Frame Received in ProcessQue
[m3video] 6982: DECODE: CH3:
[m3video] Freeing flush Frame
[m3video] 6982: IPCBITSIN:Link[1000001a]:
[m3video] Flush Frame freed for ch[3]
DecLib : in Func: InitDecDispLib at line: [803]: Encoded Stream Thread Created
[m3vpss ] 6997: DISPLAY: Start in progress !!!
[m3vpss ] 7041: DISPLAY: Start Done !!!
[m3vpss ] 7041: DISPLAY: AUX PATH: 46 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) Drop
[m3vpss ] 7042: DISPLAY DRV: AUX PATH: Q:[2] Display:[2], Repeat:[1], DQ:[0]
[m3vpss ] 7042: DISPLAY: Start in progress !!!
[m3vpss ] 7108: DISPLAY: Start Done !!!
[m3vpss ] 7108: DISPLAY: DVO2(BP1) : 15 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) D
[m3vpss ] 7108: SWMS: Start in Progress !!!
[m3vpss ] 7109: SWMS: Start Done !!!
[m3vpss ] 7109: DISPLAY DRV: DVO2(BP1) : Q:[2] Display:[1], Repeat:[0], DQ:[0]
[m3vpss ] 7109: SWMS: Start in Progress !!!
[m3vpss ] 7109: SWMS: Start Done !!!
DEVICE: TW2968: Start Done (0x80=0xbf) !!!
[m3vpss ] 7955: CAPTURE: Start in progress !!!
[m3vpss ] 8055: CAPTURE: Enabled Time Stamping !!!
[m3vpss ] 8063: CAPTURE: Start Done !!!
Disable Channel: 0
Disable Channel: 4
Disable Channel: 8
Disable Channel: 1
Disable Channel: 5
Disable Channel: 9
Disable Channel: 2
Disable Channel: 6
Disable Channel: 10
Disable Channel: 3
Disable Channel: 7
Disable Channel: 11 DEVICE: TW2968: Video Status: 0x00=0x61,CHIP STATUS:0x0d=0x00,STD_SEL: 0x0e=0x97 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
DEVICE: TW2968: Video Status: 0x10=0x87,CHIP STATUS:0x1d=0x00,STD_SEL: 0x1e=0x97 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
DEVICE: TW2968: Video Status: 0x20=0x87,CHIP STATUS:0x2d=0x00,STD_SEL: 0x2e=0x97 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
DEVICE: TW2968: Video Status: 0x30=0x87,CHIP STATUS:0x3d=0x00,STD_SEL: 0x3e=0x97 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
DecLib : in Func: getTotalCpatureChannel at line: [1018]: MAX ANALOG CHANNEL : [4]
EventLib : in Func: InitEventLib at line: [182]: Total Channel : [4]
DecLib : in Func: InitDecDispLib at line: [874]: Audio Data Thread Created
DecLib : in Func: InitDecDispLib at line: [879]: ********************* INIT Done For Liberary *****************
[host] AUDIO: CAPTURE -> Encoder creation SUCCESS for CH - 0
[host] AUDIO: CAPTURE -> Encoder creation SUCCESS for CH - 1
[host] AUDIO: CAPTURE -> Encoder creation SUCCESS for CH - 2
[host] AUDIO: CAPTURE -> Encoder creation SUCCESS for CH - 3
[host] AUDIO: Audio_startCapture() success....
[host] AUDIO: capPtr: 388920 <8192> encBuf: 38C928 <1024> encOutBuf: 0 <0> encHdl: 38DB40
[host] AUDIO: capPtr: 391458 <8192> encBuf: 38CD30 <1024> encOutBuf: 0 <0> encHdl: 38DB50
[host] AUDIO: capPtr: 395460 <8192> encBuf: 38D138 <1024> encOutBuf: 0 <0> encHdl: 38DB60
[host] AUDIO: capPtr: 399468 <8192> encBuf: 38D540 <1024> encOutBuf: 0 <0> encHdl: 38DB70
[host]
AUDIO: STARTING AUDIO CAPTURE!!!!!
[host]
AUDIO: AUDIO CAPTURE DEVICE Init Done!!!!!
[m3vpss ] CAPTURE : Capture FPS: 0.0 fps ... in 4294959.2 secs
[m3vpss ]
DEVICE: TW2968: Video Status: 0x00=0x61,CHIP STATUS:0x0d=0x00,STD_SEL: 0x0e=0x97 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
DEVICE: TW2968: Video Status: 0x10=0x97,CHIP STATUS:0x1d=0x00,STD_SEL: 0x1e=0x97 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
DEVICE: TW2968: Video Status: 0x20=0x97,CHIP STATUS:0x2d=0x00,STD_SEL: 0x2e=0xa7 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
DEVICE: TW2968: Video Status: 0x30=0x87,CHIP STATUS:0x3d=0x80,STD_SEL: 0x3e=0xa7 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
[m3vpss ] *** Capture Driver Advanced Statistics ***
[m3vpss ]
[m3vpss ] VIP Parser Reset Count : 0
[m3vpss ]
[m3vpss ] | Total Even Odd Total Even Odd Min / Max Min / Max Dropped Fid Repeat Frame Error Y/C
[m3vpss ] CH | Fields Fields Fields FPS FPS FPS Width Height Fields Count (Desc Error Y/C)
[m3vpss ] TILER_STATS: CNT :8BIT
[m3vpss ] TILER_STATS: CNT RESOLUTION: 16384 x 3072
[m3vpss ] TILER_STATS: BUCKET RESOLUTION: 16384 x 3068
[m3vpss ] TILER_STATS: NUM FREE BUCKETS: 0
[m3vpss ] TILER_STATS: NUM USED BUCKETS: 1
[m3vpss ] TILER_STATS: TOTAL FREE AREA: 40583168 (80 %)
[m3vpss ] TILER_STATS: TOTAL USED AREA: 9682944 (19 %)
[m3vpss ] TILER_STATS: TOTAL WASTE AREA: 229376 (0 %)
[m3vpss ] TILER_STATS: MAX WIDTH RECT: 16384 x 1180
[m3vpss ] TILER_STATS: CNT :16BIT
[m3vpss ] TILER_STATS: CNT RESOLUTION: 32768 x 1024
[m3vpss ] TILER_STATS: BUCKET RESOLUTION: 32768 x 1024
[m3vpss ] TILER_STATS: NUM FREE BUCKETS: 0
[m3vpss ] TILER_STATS: NUM USED BUCKETS: 1
[m3vpss ] TILER_STATS: TOTAL FREE AREA: 28712960 (85 %)
[m3vpss ] TILER_STATS: TOTAL USED AREA: 4841472 (14 %)
[m3vpss ] TILER_STATS: TOTAL WASTE AREA: 114688 (0 %)
[m3vpss ] TILER_STATS: MAX WIDTH RECT: 32768 x 400
[m3vpss ] TILER_STATS: MAX HEIGHT RECT: 32768 x 400
[m3vpss ]
[m3vpss ] 8450: CAPTURE: Fields = 0 (fps = 0, CPU Load = 0)
[m3vpss ] 8450: CAPTURE: Num Resets = 0 (Avg 0 ms per reset)
[m3vpss ] 8450: SYSTEM : FREE SPACE : System Heap = 244216 B, Mbx = 10240 msgs)
[m3vpss ] 8450: SYSTEM : FREE SPACE : SR0 Heap = 240512 B (0 MB)
[m3vpss ] 8450: SYSTEM : FREE SPACE : Frame Buffer = 6057728 B (5 MB)
[m3vpss ] 8451: SYSTEM : FREE SPACE : Bitstream Buffer = 52643968 B (50 MB)
[m3vpss ] TILER_STATS: CNT :8BIT
[m3vpss ] TILER_STATS: CNT RESOLUTION: 16384 x 3072
[m3vpss ] *** Capture List Manager Advanced Statistics ***
[m3vpss ]
[m3vpss ] List Post Count : 67
[m3vpss ] List Stall Count : 0
DEVICE: TW2968: Video Status: 0x00=0x79,CHIP STATUS:0x0d=0x10,STD_SEL: 0x0e=0x17 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
TW2968: Video Is Detected
DEVICE: TW2968: Video Status: 0x10=0x97,CHIP STATUS:0x1d=0x00,STD_SEL: 0x1e=0x27 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
DEVICE: TW2968: Video Status: 0x20=0x97,CHIP STATUS:0x2d=0x80,STD_SEL: 0x2e=0x27 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
[m3vpss ] List Post Time (ms) : Max = 0, Min = 0, Avg = 0, Total = 0
DEVICE: TW2968: Video Status: 0x30=0x97,CHIP STATUS:0x3d=0x80,STD_SEL: 0x3e=0x27 !!!
DEVICE: TW2968: VIDEO AND AUDIO STATUS: 0xfd=0x01 !!!
[m3vpss ] INTC Timeout Count : (0, 0) (Min timeout value = 988, 1000)
[m3vpss ] Descriptor miss found count : 0
[m3vpss ]
[m3vpss ]
[m3vpss ] VIP and VPDMA registers,
[m3vpss ] VIP0 : FIQ_STATUS : 0x4810551c = 0x00000000
[m3vpss ] VIP1 : FIQ_STATUS : 0x48105a1c = 0x00000000
[m3vpss ] | Total Even Odd Total Even Odd Min / Max Min / Max Dropped Fid Repeat Frame Error Y/C
[m3vpss ] CH | Fields Fields Fields FPS FPS FPS Width Height Fields Count (Desc Error Y/C)
[m3vpss ] ------------------------------------------------------------------------------------------------------------
[m3vpss ]
[m3vpss ] VIP Capture Port 0 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescMissMatch3 = 0
[m3vpss ]
[m3vpss ] *** Capture List Manager Advanced Statistics ***
[m3vpss ]
[m3vpss ] List Post Count : 83
[m3vpss ] List Stall Count : 0
[m3vpss ] List Post Time (ms) : Max = 0, Min = 0, Avg = 0, Total = 0
[m3vpss ] INTC Timeout Count : (0, 0) (Min timeout value = 988, 1000)
[m3vpss ] TILER_STATS: CNT :16BIT
[m3vpss ] TILER_STATS: CNT RESOLUTION: 32768 x 1024
[m3vpss ] TILER_STATS: BUCKET RESOLUTION: 32768 x 1024
[m3vpss ] TILER_STATS: NUM FREE BUCKETS: 0
[m3vpss ] TILER_STATS: NUM USED BUCKETS: 1
[m3vpss ] TILER_STATS: TOTAL FREE AREA: 28712960 (85 %)
[m3vpss ] TILER_STATS: TOTAL USED AREA: 4841472 (14 %)
[m3vpss ]
[m3vpss ] 8962: CAPTURE: Fields = 0 (fps = 0, CPU Load = 0)
[m3vpss ] 8962: CAPTURE: Num Resets = 0 (Avg 0 ms per reset)
[m3vpss ] 8962: SYSTEM : FREE SPACE : System Heap = 244216 B, Mbx = 10240 msgs)
[m3vpss ] 8962: SYSTEM : FREE SPACE : SR0 Heap = 240512 B (0 MB)
[m3vpss ] 8962: SYSTEM : FREE SPACE : Frame Buffer = 6057728 B (5 MB)
[m3vpss ] 8963: SYSTEM : FREE SPACE : Bitstream Buffer = 52643968 B (50 MB)
[m3vpss ] TILER_STATS: CNT :8BIT
[m3vpss ] TILER_STATS: CNT :8BIT
Spot App : Func: main at line: [531]: Video Standard : [1] & board type:[0]
[m3vpss ] TILER_STATS: CNT RESOLUTION: 16384 x 3072
[m3vpss ] TILER_STATS: BUCKET RESOLUTION: 16384 x 3068
[m3vpss ] TILER_STATS: NUM FREE BUCKETS: 0
Sorry for Lots of Debugging Message from my side also.