This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Transferring 600 MSPS Data from FPGA to OMAP-L138 via uPP

Expert 2370 points
Other Parts Discussed in Thread: OMAP-L138, ADS5282

Hi,

I have 8 channel, 12 bits, 50 MHz A/D converter connected to Altera DE2-115 FPGA. I want to transfer the data from each channel one by one to OMAP-L138 for signal processing. Is it even possible to transfer 600 MSPS data of each channel from Altera DE2-115 FPGA to OMAP-L138 via uPP ?

Is there any connector which connects uPP to FPGA ? If not, can you tell me what should be done in terms of hardware to make the connection ? 

Thanks.

-BAS