I was wondering if the ROM boot loader source for the C665x has been released yet? I checked the wiki and only the C6670 and C6678 RBL source are listed.
Thanks,
Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I was wondering if the ROM boot loader source for the C665x has been released yet? I checked the wiki and only the C6670 and C6678 RBL source are listed.
Thanks,
Mark
Hi Mark ,
The PG 1.0 release of the C6657 ROM will be available on ti.com this week. I will post an update here once it is available.
Regards,
Rahul
Hi Rahul,
Thanks for the response, is there any update on when it will be available?
Mark