Other Parts Discussed in Thread: OMAP3503
Hi,
Did anyone got the USB interface of the OMAP3503 EVM working with Linux ? I want to connect a USB sound card, and it just does nothing.
I do not get a USB event when I plug in any USB device. Just nothing happens. The USB Host driver is built in, detects one HUB Root,
but thats it.
As far as I understand, I need a "Mini A" cable, with the ID pin tied to ground. Can anyone confirm if this is correct ?
Best Regards,
Manuel
(Sorry for the wrong post in the DM355 board, I think here maybe is the right place).