This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XAM3359 (720 MHz Turbo) Boot ROM replacement .mac for EWARM

See http://e2e.ti.com/support/embedded/starterware/f/790/p/298458/1055332.aspx#1055332
for the background.
I need a .mac debugger script for IAR EWARM that does the setup that the XAM3359
boot ROM does when booting through the boot ROM. I cannot boot through the boot
ROM because no boot mode is implemented on my board, which otherwise is modeled
after the EVM SK. I took a look at the .mac files provided in Starterware in
C:\ti\AM335X_StarterWare\tools\ewarm\ but they don't configure the L3 OCMC RAM,
for example; they replicate the job of the MLO/Bootloader. Since I am
implementing the MLO/Bootloader, I only need a .mac that replaces what the boot
ROM does. Can I have this?
My crystal frequency is 24 MHz and the XAM3359 is running at 720 MHz.
Thanks.