This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Rebuilding HUA Demo on C6670

Hello all,

I am using CCS 5.2 along with MCSDK 2.0.3.15, NDK 2.20.4.26, PDK 1.0.0.15 and XDC 3.22.1.21. If I load the pre-installed .out file from the release folder everything works fine and I am able to ping the board. However if I rebuild the .out file either in debug or release mode I can not ping the evm board although I am getting no compilation errors. Is there any known bug or do I miss some setting in CCS to make it work? I appreciate any help in this issue, thanks in advance!

Best Regards

Burak

P.S: By the way updating solves the problem but is not a solution as our code has to be compliant in the versions to the code of our partners in the project!