I want to complete external display by PCIe port after decoding.
Now the output of swms link should be the mapping address of the PCIe port, and the following link of the swms link is NULL link, instead of the display link.
There are some questions about the PCIe port:
1.What should be the mapping address of PCIe? In DVR_RDK4.0, How could I get it? Could you explain which files are involved in PCIe port physical and virtual mapping address?
2. Could M3 access the address of PCIe mapping address directly? What's the differences between the M3 and A8 access of the PCIe address?
Thanks.