I want to send data from dsp1 to dsp2 by using message, when the receiver get the data successfully, there is an interrupt being triggerred. But the problem is, the receiver can only receive the data from the sender 4 times. So I have to power down the DSP and then power it up, then the message can work. I dont not know why this happen and how to solve this problem.
Here is the project which has the problem, Who can fix it or tell to do solve the problem.
thank you very much and I am very appreciate for your help.