Hello,
we are currently facing a problem with the initialization of the McASP0 of a C6727. We want to transmit data using the CPU to writte into the XBUF0 whenever the correponding flag indicates a ready signal. Initialization for the format seems to be fine, as we have clocks and the frame signal also fits our configuration. The code is attached, here is only the current part where we initialize. It's also interesting to see that it will never transmitt when free runnning, and only once if we step through the init manually. It never transmits when we are in the while(1) loop in the main. This makes us suspect that there is something wrong with the clocks, but we tried several different settings and combinations for the clock dividers, without success. The attached pictures show the one transmission we get when stepping manualy, which looks just fine, but then the second picture shows the signals at normal operation. Green is XCLK0, blue the frame sync, and yellow the AXR0. The transmission sends 0x5F0AF50 as expected, but only in frame 0, nothing in frame 1. We tried the burst mode, which works fine, and more frames, but they don't transmitt as well.
void initMcASP0(void)
{
McASP0[GBLCTL]=0x0;
McASP0[PWRDEMU]=0x1;
McASP0[XMASK]=0xFFFFFFFF; // No replacing of Bits
McASP0[XFMT]= 0x80F8; // 00 delay, 1 MSB First, 0 Pad, 0 value, 0xF SlotSize 32, 1 Peripheral Bus, 000 no rotation
McASP0[AFSXCTL]= 0x112; // 0x2 Slots, 00 reserved, 1 Word, 00 reserved, 1 internal, 0 rising edge
McASP0[ACLKXCTL]= 0x3F; // 0 rising edge, 0 Sync, 1 internal, 0x1F Divide by 32
McASP0[AHCLKXCTL]= 0x8000; // 1 internal, 0 rising edge, 00 reserved, 0 divide AUXCLK by 1
McASP0[XTDM]= 0x1; // slots 0 and 1 active
McASP0[XINTCTL]= 0x0; // no interrupts
McASP0[XCLKCHK]= 0xFF0005; // 0xFF maximum, 0x00 minimum, 0 autoswitch disabled, 000 reserved, 0x5 prescaler 32
McASP0[SRCTL0]= 0x1; // 0 RRDY, 0 XRDY, 0 3-State, 01 Transmitter
McASP0[PFUNC]= 0x0; // McASP occupies all Pins
McASP0[PDIR]= McASP0[PDIR] | 0x1E00000F; // 1E00000F Frame Sync, HCLK, CLK, AMUTE AXR0-7 as Outputs for McASP0
McASP0[DITCTL]= 0x0; // DIT mode disabled
McASP0[DLBCTL]= 0x0; // Loopback disabled
McASP0[AMUTE]= 0x0; // AMUTE disabled
McASP0[GBLCTL]= McASP0[GBLCTL] | 0x202; // Enable RHCLK and XHCLK
while(!(McASP0[GBLCTL] & 0x202));
McASP0[GBLCTL]= McASP0[GBLCTL] | 0x101; // Enable RCLK and XCLK
while(!(McASP0[GBLCTL] & 0x101));
McASP0[XSTAT]= 0xFFFF; // Clear all status registers
McASP0[RSTAT]= 0xFFFF;
McASP0[GBLCTL]= McASP0[GBLCTL] | 0x404; // Enable Serializers
while(!(McASP0[GBLCTL] & 0x404));
McASP0[XBUF0]= 0x5F0AF50A; // Sending AAAA in the first comand
McASP0[GBLCTL]= McASP0[GBLCTL] | 0x808; // Enable State Machines
while(!(McASP0[GBLCTL] & 0x808));
McASP0[GBLCTL]= McASP0[GBLCTL] | 0x1010; // Enable Frame Syncs
while(!(McASP0[GBLCTL] & 0x1010));
while((McASP0[SRCTL0] & 0x00000010) != 0x00000010);
}
int main(void) {
initMcASP0();
while(1)
{
while((McASP0[SRCTL0] & 0x00000010) != 0x00000010);
McASP0[XBUF0]=0xBEEF;
}
return 0;
}
The transmission when steping manually:
The "normal" operation (using 2 frames, 32 Bit, Sync duration 1 word):
Does somebody know what do we do wrong in the initialization, that it does not transmitt continuously when we feed the buffer with the CPU? We would expect something similar to the burst mode, which works fine. Thank you very much for your help!
/*
* main.c
*/
extern far int McASP0[0x2BF];
extern far int McASP1[0x2BF];
extern far int McASP2[0x2BF];
#define GBLCTL (0x44/4)
#define PWRDEMU (0x04/4)
#define RMASK (0x64/4)
#define RFMT (0x68/4)
#define AFSRCTL (0x6C/4)
#define ACLKRCTL (0x70/4)
#define AHCLKRCTL (0x74/4)
#define RTDM (0x78/4)
#define RINTCTL (0x7C/4)
#define RCLKCHK (0x88/4)
#define XMASK (0xA4/4)
#define XFMT (0xA8/4)
#define AFSXCTL (0xAC/4)
#define ACLKXCTL (0xB0/4)
#define AHCLKXCTL (0xB4/4)
#define XTDM (0xB8/4)
#define XINTCTL (0xBC/4)
#define XCLKCHK (0xC8/4)
#define SRCTL0 (0x180/4)
#define SRCTL1 (0x184/4)
#define SRCTL2 (0x188/4)
#define SRCTL3 (0x18C/4)
#define SRCTL4 (0x190/4)
#define SRCTL5 (0x194/4)
#define SRCTL6 (0x198/4)
#define SRCTL7 (0x19C/4)
#define SRCTL8 (0x1A0/4)
#define SRCTL9 (0x1A4/4)
#define SRCTL10 (0x1A8/4)
#define SRCTL11 (0x1AC/4)
#define SRCTL12 (0x1B0/4)
#define SRCTL13 (0x1B4/4)
#define SRCTL14 (0x1B8/4)
#define SRCTL15 (0x1BC/4)
#define PFUNC (0x10/4)
#define PDIR (0x14/4)
#define DITCTL (0x50/4)
#define DLBCTL (0x4C/4)
#define AMUTE (0x48/4)
#define XSTAT (0xC0/4)
#define RSTAT (0x80/4)
#define XBUF0 (0x200/4)
#define XBUF1 (0x204/4)
#define XBUF2 (0x208/4)
#define XBUF3 (0x20C/4)
#define XBUF4 (0x210/4)
#define XBUF5 (0x214/4)
#define XBUF6 (0x218/4)
#define XBUF7 (0x21C/4)
#define XBUF8 (0x220/4)
#define XBUF9 (0x224/4)
#define XBUF10 (0x228/4)
#define XBUF11 (0x22C/4)
#define XBUF12 (0x230/4)
#define XBUF13 (0x234/4)
#define XBUF14 (0x238/4)
#define XBUF15 (0x23C/4)
#define RBUF0 (0x280/4)
#define RBUF1 (0x284/4)
#define RBUF2 (0x288/4)
#define RBUF3 (0x28C/4)
#define RBUF4 (0x290/4)
#define RBUF5 (0x294/4)
#define RBUF6 (0x298/4)
#define RBUF7 (0x29C/4)
#define RBUF8 (0x2A0/4)
#define RBUF9 (0x2A4/4)
#define RBUF10 (0x2A8/4)
#define RBUF11 (0x2AC/4)
#define RBUF12 (0x2B0/4)
#define RBUF13 (0x2B4/4)
#define RBUF14 (0x2B8/4)
#define RBUF15 (0x2BC/4)
void initMcASP0(void)
{
McASP0[GBLCTL]=0x0;
McASP0[PWRDEMU]=0x1;
McASP0[XMASK]=0xFFFFFFFF; // No replacing of Bits
McASP0[XFMT]= 0x80F8; // 00 delay, 1 MSB First, 0 Pad, 0 value, 0xF SlotSize 32, 1 Peripheral Bus, 000 no rotation
McASP0[AFSXCTL]= 0x112; // 0x2 Slots, 00 reserved, 1 Word, 00 reserved, 1 internal, 0 rising edge
McASP0[ACLKXCTL]= 0x3F; // 0 rising edge, 0 Sync, 1 internal, 0x1F Divide by 32
McASP0[AHCLKXCTL]= 0x8000; // 1 internal, 0 rising edge, 00 reserved, 0 divide AUXCLK by 1
McASP0[XTDM]= 0x1; // slots 0 and 1 active
McASP0[XINTCTL]= 0x0; // no interrupts
McASP0[XCLKCHK]= 0xFF0005; // 0xFF maximum, 0x00 minimum, 0 autoswitch disabled, 000 reserved, 0x5 prescaler 32
McASP0[SRCTL0]= 0x1; // 0 RRDY, 0 XRDY, 0 3-State, 01 Transmitter
McASP0[PFUNC]= 0x0; // McASP occupies all Pins
McASP0[PDIR]= McASP0[PDIR] | 0x1E00000F; // 1E00000F Frame Sync, HCLK, CLK, AMUTE AXR0-7 as Outputs for McASP0
McASP0[DITCTL]= 0x0; // DIT mode disabled
McASP0[DLBCTL]= 0x0; // Loopback disabled
McASP0[AMUTE]= 0x0; // AMUTE disabled
McASP0[GBLCTL]= McASP0[GBLCTL] | 0x202; // Enable RHCLK and XHCLK
while(!(McASP0[GBLCTL] & 0x202));
McASP0[GBLCTL]= McASP0[GBLCTL] | 0x101; // Enable RCLK and XCLK
while(!(McASP0[GBLCTL] & 0x101));
McASP0[XSTAT]= 0xFFFF; // Clear all status registers
McASP0[RSTAT]= 0xFFFF;
McASP0[GBLCTL]= McASP0[GBLCTL] | 0x404; // Enable Serializers
while(!(McASP0[GBLCTL] & 0x404));
McASP0[XBUF0]= 0x5F0AF50A; // Sending AAAA in the first comand
McASP0[GBLCTL]= McASP0[GBLCTL] | 0x808; // Enable State Machines
while(!(McASP0[GBLCTL] & 0x808));
McASP0[GBLCTL]= McASP0[GBLCTL] | 0x1010; // Enable Frame Syncs
while(!(McASP0[GBLCTL] & 0x1010));
while((McASP0[SRCTL0] & 0x00000010) != 0x00000010);
}
int main(void) {
initMcASP0();
while(1)
{
while((McASP0[SRCTL0] & 0x00000010) != 0x00000010);
McASP0[XBUF0]=0xBEEF;
}
return 0;
}