This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x eMMC detection problem

Hi

We are using Micron eMMC on MMC0. I can access eMMC with U-Boot, but kernel can’t detect eMMC. (I set gpio_cd, gpio_wp to -EINVAL and it's 4 bit mode same as beaglebone uSD)

I am using “linux-3.2.0-psp04.06.00.11”and board boots from SPI Flash. 

Regards