Hi everyone,
Now, I attempt to make C6457 to visit a SWITCH(cps1432) through the SRIO BUS. By means of configuring the LSU0~LSU5 registers, the C6457 one core sends a "Maintenance READ" request to the SWITCH for the Device Identity CAR of SWITCH which is get back from the response packet.
But, now the work is failed, the Lsu6 is 0x06 as a error: "Transaction complete, non-posted response packet (type 8 and 13) contained ERROR status, or response payload length was in error".
So, I want to konw the reason, and what can i do.
Thanks for help.
Lew