This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VGA YPbPr Ghost Image

Hi, TIers

I'm using DM8168 with RDK 3.0

There is ghost image in my VGA/YPbPr output, issue and my privious attempting are described in

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/302687/1060719.aspx#1060719

Now, I have one evaluation board from TI's 3rd party, its YPbPr output works properly,

so , I compared values of 53 HDVPSS-HD-VENC registers between them, and I noticed the disparity just in one register(with address 0x48108048), the value of our board is 0x05003000, the 3rd party's is 0x05004000,

According to the NDA datasheet

"DigitalMediaProcessors High-DefinitionVideoProcessingSubsystem(HDVPSS)TechnicalReferenceManual"

it means the starting location of the VS pulse in a frame, ours' is 0x03, the other board is 0x04;

I don't know the exact meaning of these values,

and I want to replace the value of the register on our board with the other's to do a try, how can I do this?

Appreciate with any reply!