We are looking at using the AM37xx family. The only function we need from the TPS support chips are the DC/DC converters. The question is, can we use other DC/DC converters that do not support TI's "SmartReflex" functionality?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are looking at using the AM37xx family. The only function we need from the TPS support chips are the DC/DC converters. The question is, can we use other DC/DC converters that do not support TI's "SmartReflex" functionality?
Hi John,
The usage of the Smart Reflex is not at 100 % mandatory but it is recommended because:
The variations in the silicon manufacturing processes are responsible for the difference in performance and/or power consumption of the device. Adaptive Voltage Scaling - AVS, implemented with SmartReflex(TM) technology, tends to narrow this difference.
Dedicated SmartReflex hardware implements a feedback loop - without processor intervention - which optimizes the voltage levels to account for differences in the manufacturing process, temperature and silicon degradation.
The processor ROM code expects that the Smart Reflex hardware is active and if it doesn't work some errors will appear.
If the AM37xx processor in your board works at high frequency (nearly 1 GHz) its operating life will decrease considerably.
If you are searching for less expensive DC/DC converter for your board I suggest you to search for some decision posting new thread in the Non-Isolated DC/DC Section of the TI E2E Support Community at the link:
http://e2e.ti.com/support/power_management/non-isolated_dcdc/default.aspx
Therefore I suggest you to use a DC/DC converter which supports SmartReflex(TM) technology.
BR
Tsvetolin Shulev
Hi John,
I addition to previous post I suggest you link with useful description of advantages of the SmartReflex(TM) technology:
BR
Tsvetolin Shulev