I've been searching the forums all day and also reading the c6x linux user's guide. I want to make sure I understand this correctly.
I am able to get through a build of c6x and now I want to download to the 6678 EVM board.
From what I've read, to download to NAND using the USB/JTAG interface you must have CCS.
The other option is TFTP. This is mentioned in the user's guide but not fully explained.
Can anyone tell me (or point me to a document) that shows how to download an image to the EVM from the host command line? In my /product directory, after I build I have the following files:
gplv3-devtools-c6x-hf.cpio.gz
min-root-c6x-hf.cpio.gz
mcsdk-demo-root-c6x-hf.cpio.gz
modules-2.6.34-evmc6678.el-dev-agsc6x2-20131125.tar.gz
evmc6678-initramfs-demo.el-hf-dev-agsc6x2-20131125.cpio.gz
evmc6678-initramfs-demo.el-hf-dev-agsc6x2-20131125.bin
evmc6678-initramfs-min.el-hf-dev-agsc6x2-20131125.cpio.gz
evmc6678-initramfs-min.el-hf-dev-agsc6x2-20131125.bin
Thanks, MS