Hi Experts,
I am using Dm6446 on mvl401( linux 2.6.10), when the image up, the MUSB Host can not detect any usb devcies.
I checked the debug message, just found that there even is no connection interrupt.
we add one workaround to force the host controller to route to ' A device' by set HOSTREQ bit in DEVCTL register in musb_start routine,
the connection interrupt coming, and can detect the plugged devcies. But the issue is when the usb device plugged out, host controller
can not detect the disconnection (_no_ disconnection interrupt), the controller gose to the suspend stage. I checked the vbus, the stage is ok too.
I search the community and the davinci maillist, no found such issue as mine.
I do not know it is my hardware issue or something else?
Any suggestions will be very appreciated!
Thanks very much and Merry Christmas,
Tomas