Other Parts Discussed in Thread: TWL6030, WL1271
Hi,
I would like to enable RPmsg on my pandaboard ES omap4460 using Android. Following these instructions http://omappedia.org/wiki/RPMsg_Tesla I managed to generate a tesla-dsp.bin, a ducati-m3.bin and the uImage with rpmsg built-in. (kernel 3.0). Unfortunately, after copying the two binary files in the firmware directory and after replacing the uImage in the boot directory, I get some errors when booting on the pandaboard. I tried with two different versions of android (linaro 13.10 running a 4.3 android and linaro 12.01 using a 4.0android)
Any idea what am I doing wrong? heres the boot log:
Texas Instruments X-Loader 1.41 (Jan 24 2012 - 10:05:52)
OMAP4460: 1.2 GHz capable SOM
mmc read: Invalid size
Starting OS Bootloader from MMC/SD1 ...
U-Boot 2011.06 (Aug 20 2011 - 18:00:16)
CPU : OMAP4430
Board: OMAP4 Panda
I2C: ready
DRAM: 1 GiB
MMC: OMAP SD/MMC: 0
Using default environment
In: serial
Out: serial
Err: serial
Net: No ethernet found.
Hit any key to stop autoboot: 3 2 1 0
reading boot.scr
498 bytes read
Running bootscript from mmc0 ...
## Executing script at 82000000
reading uImage
3634964 bytes read
reading uInitrd
161812 bytes read
reading board.dtb
** Unable to read "board.dtb" from mmc 0:1 **
## Booting kernel from Legacy Image at 80200000 ...
Image Name: Linux-3.0.31-01923-g519bdcb-dirt
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3634900 Bytes = 3.5 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 81600000 ...
Image Name: Android Ramdisk Image
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 161748 Bytes = 158 KiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
ERROR: Did not find a cmdline Flattened Device Tree
Could not find a valid device tree
reading uImage
3634964 bytes read
Booting from mmc0 ...
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-3.0.31-01923-g519bdcb-dirt
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3634900 Bytes = 3.5 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Linux version 3.0.31-01923-g519bdcb-dirty (qpesquet@brenthis1) (gcc version 4.7.4 20131014 (prerelease) (Linaro GCC 4.7-2013.10) ) #2 SMP PREEMPT Fri Nov 22 18:05:09 EET 2013
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: OMAP4 Panda board
[ 0.000000] Truncating RAM at 80000000-bfffffff to -afffffff (vmalloc region overlap).
[ 0.000000] omap4_total_ram_size = 0x30000000
[ 0.000000] omap4_smc_size = 0x300000
[ 0.000000] omap4_ion_heap_secure_input_size = 0x5a00000
[ 0.000000] omap4_ion_heap_secure_output_wfdhdcp_size = 0x1000000
[ 0.000000] omap4_ducati_heap_size = 0x6d00000
[ 0.000000] omap4_ion_heap_tiler_mem_size = 0x0
[ 0.000000] omap4_ion_heap_nonsec_tiler_mem_size = 0x0
[ 0.000000] omap4_smc_addr = 0xafd00000
[ 0.000000] omap4_ion_heap_secure_input_addr = 0xaa300000
[ 0.000000] omap4_ion_heap_secure_output_wfdhdcp_addr = 0xa9300000
[ 0.000000] omap4_ducati_heap_addr = 0xa2600000
[ 0.000000] omap4_ion_heap_tiler_mem_addr = 0xa2600000
[ 0.000000] omap4_ion_heap_nonsec_tiler_mem_addr = 0xa2600000
[ 0.000000] omap_ion_init: secure_input id=2 [aa300000-afd00000] size=5a00000
[ 0.000000] omap_ion_init: secure_output_wfdhdcp id=5 [a9300000-aa300000] size=1000000
[ 0.000000] omap_ion_init: tiler id=1 [a2600000-a2600000] size=0
[ 0.000000] omap_ion_init: nonsecure_tiler id=3 [a2600000-a2600000] size=0
[ 0.000000] omap_ion_init: system id=0 [0-0] size=0
[ 0.000000] omap_ion_init: tiler_reservation id=4 [0-0] size=0
[ 0.000000] Reserving 16777216 bytes SDRAM for VRAM
[ 0.000000] Memory policy: ECC disabled, Data cache writealloc
[ 0.000000] OMAP4460 ES1.1
[ 0.000000] SRAM: Mapped pa 0x40300000 to va 0xfe400000 size: 0xd000
[ 0.000000] On node 0 totalpages: 134656
[ 0.000000] free_area_init_node: node 0, pgdat c0735b20, node_mem_map c0880000
[ 0.000000] Normal zone: 1536 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 133120 pages, LIFO batch:31
[ 0.000000] PERCPU: Embedded 7 pages/cpu @c0e8a000 s6944 r8192 d13536 u32768
[ 0.000000] pcpu-alloc: s6944 r8192 d13536 u32768 alloc=8*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 133120
[ 0.000000] Kernel command line: console=ttyO2,115200n8 mem=1G androidboot.console=ttyO2 console=ttyS2,115200n8 vram=16M root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 256MB 270MB = 526MB total
[ 0.000000] Memory: 522888k/522888k available, 263544k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
[ 0.000000] vmalloc : 0xf0800000 - 0xf8000000 ( 120 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .init : 0xc0008000 - 0xc0047000 ( 252 kB)
[ 0.000000] .text : 0xc0047000 - 0xc06d4000 (6708 kB)
[ 0.000000] .data : 0xc06d4000 - 0xc0736300 ( 393 kB)
[ 0.000000] .bss : 0xc0736340 - 0xc087f920 (1318 kB)
[ 0.000000] SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:410
[ 0.000000] omap_hwmod: dpll_mpu_m2_ck: missing clockdomain for dpll_mpu_m2_ck.
[ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000030] Calibrating delay loop... 1830.74 BogoMIPS (lpj=7151616)
[ 0.070373] pid_max: default: 32768 minimum: 301
[ 0.070373] Mount-cache hash table entries: 512
[ 0.070373] Initializing cgroup subsys debug
[ 0.070373] Initializing cgroup subsys cpuacct
[ 0.071289] Initializing cgroup subsys freezer
[ 0.071350] CPU: Testing write buffer coherency: ok
[ 0.071777] L310 cache controller enabled
[ 0.071807] l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x5e470000, Cache size: 1048576 B
[ 0.149932] CPU1: Booted secondary processor
[ 0.220275] Brought up 2 CPUs
[ 0.220275] SMP: Total of 2 processors activated (3670.89 BogoMIPS).
[ 0.220458] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for emif_fw
[ 0.220458] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l3_instr
[ 0.222900] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l3_main_1
[ 0.222900] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l3_main_2
[ 0.222930] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_abe
[ 0.222930] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_cfg
[ 0.222930] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_per
[ 0.222961] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_wkup
[ 0.222961] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for mpu_private
[ 0.223022] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for sl2if
[ 0.223022] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for thermal_sensor
[ 0.223022] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for usbhs_ohci
[ 0.223083] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for usbhs_ehci
[ 0.223083] omap_hwmod: l3_div_ck: missing clockdomain for l3_div_ck.
[ 0.223083] omap_hwmod: l4_div_ck: missing clockdomain for l4_div_ck.
[ 0.225219] _omap4_module_wait_ready: Timeout waiting for module enable (mcpdm_fck: clkctrl = 0x30002)
[ 0.228088] omap_hwmod: mcpdm: cannot be enabled (3)
[ 0.233062] print_constraints: dummy:
[ 0.233062] NET: Registered protocol family 16
[ 0.233734] GPMC revision 6.0
[ 0.233734] EMIF0 is enabled with IRQ142
[ 0.233734] EMIF1 is enabled with IRQ143
[ 0.234741] Last reset was cold reset (PRM_RSTST=0x1)
[ 0.234741]
[ 0.235107] OMAP GPIO hardware version 0.1
[ 0.236022] omap_mux_init: Add partition: #1: core, flags: 2
[ 0.236022] omap_mux_init: Add partition: #2: wkup, flags: 2
[ 0.238281] omap_mux_get_by_name: Could not find signal uart1_cts.uart1_cts
[ 0.238281] omap_hwmod_mux_init: Could not allocate device mux entry
[ 0.244140] OMAP DMA hardware revision 0.0
[ 0.244140] omap_rproc_get_pool: dsp - static memory is unavailable: 0x0, 0x0
[ 0.244140] omap_rproc_get_pool: ipu - carveout memory is unavailable: 0x0, 0x0
[ 0.250183] bio: create slab <bio-0> at 0
[ 0.250488] print_constraints: vwl1271: 1800 mV
[ 0.250488] i2c-core: driver [twl] using legacy suspend method
[ 0.251068] i2c-core: driver [twl] using legacy resume method
[ 0.251068] SCSI subsystem initialized
[ 0.251495] usbcore: registered new interface driver usbfs
[ 0.251495] usbcore: registered new interface driver hub
[ 0.251708] usbcore: registered new device driver usb
[ 0.252319] omap_i2c omap_i2c.1: bus 1 rev4.0 at 400 kHz
[ 0.252838] Skipping twl internal clock init and using bootloader value (unknown osc rate)
[ 0.253295] twl6030: PIH (irq 39) chaining IRQs 368..387
[ 0.255371] machine_constraints_voltage: VUSB: failed to apply 3300000uV constraint
[ 0.255371] twl_reg twl_reg.46: can't register VUSB, -22
[ 0.255371] twl_reg: probe of twl_reg.46 failed with error -22
[ 0.255767] twl6030_usb twl6030_usb: ldo init failed
[ 0.256225] print_constraints: VMMC: 1200 <--> 3000 mV at 3000 mV normal standby
[ 0.256622] print_constraints: VPP: 1800 <--> 2500 mV at 1900 mV normal standby
[ 0.256713] print_constraints: VCXIO: 1800 mV normal standby
[ 0.256988] print_constraints: VDAC: 1800 mV normal standby
[ 0.257629] print_constraints: VAUX2_6030: 1200 <--> 2800 mV at 1800 mV normal standby
[ 0.258087] print_constraints: VAUX3_6030: 1000 <--> 3000 mV at 1200 mV normal standby
[ 0.258422] print_constraints: VANA: 2100 mV normal standby
[ 0.259185] print_constraints: CLK32KG:
[ 0.259399] omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz
[ 0.259613] omap_i2c omap_i2c.3: bus 3 rev4.0 at 100 kHz
[ 0.259857] omap_i2c omap_i2c.4: bus 4 rev4.0 at 400 kHz
[ 0.259857] omap-rproc omap-rproc.0: dsp is available
[ 0.259857] omap-rproc omap-rproc.1: ipu is available
[ 0.259857] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.259857] Bluetooth: Core ver 2.16
[ 0.261047] NET: Registered protocol family 31
[ 0.261108] Bluetooth: HCI device and connection manager initialized
[ 0.261108] Bluetooth: HCI socket layer initialized
[ 0.261108] Bluetooth: L2CAP socket layer initialized
[ 0.261108] Bluetooth: SCO socket layer initialized
[ 0.261505] cfg80211: Calling CRDA to update world regulatory domain
[ 0.261627] Switching to clocksource 32k_counter
[ 0.263793] musb-hdrc: version 6.0, musb-dma, peripheral
[ 0.263793] HS USB OTG: no transceiver configured
[ 0.263885] musb-hdrc musb-hdrc: musb_init_controller failed with status -19
[ 0.264007] NET: Registered protocol family 2
[ 0.264007] IP route cache hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.264007] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
[ 0.264007] TCP bind hash table entries: 32768 (order: 7, 786432 bytes)
[ 0.264007] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.264007] TCP reno registered
[ 0.266754] UDP hash table entries: 512 (order: 3, 32768 bytes)
[ 0.266815] UDP-Lite hash table entries: 512 (order: 3, 32768 bytes)
[ 0.267150] Switched to NOHz mode on CPU #0
[ 0.267150] Switched to NOHz mode on CPU #1
[ 0.267333] NET: Registered protocol family 1
[ 0.886566] omap_init_opp_table: no hwmod or odev for hsi, [22] cannot add OPPs.
[ 0.886779] omap_init_opp_table: no hwmod or odev for hsi, [23] cannot add OPPs.
[ 1.277923] ram_console: got buffer at 90000000, size 200000
[ 1.277923] ram_console: uncorrectable error in header
[ 1.278808] ram_console: no valid data in buffer (sig = 0xbe9a080e)
[ 1.278808] console [ram-1] enabled
[ 1.293334] omap-iommu omap-iommu.0: ducati registered
[ 1.293334] omap-iommu omap-iommu.1: tesla registered
[ 1.298614] ashmem: initialized
[ 1.303405] fuse init (API version 7.16)
[ 1.303405] msgmni has been set to 1021
[ 1.307159] io scheduler noop registered
[ 1.307250] io scheduler deadline registered
[ 1.307250] io scheduler cfq registered (default)
[ 1.307525] start plist test
[ 1.316772] end plist test
[ 1.317535] OMAP DSS rev 4.0
[ 1.319061] Keyboard driver not present
[ 1.319610] dsscomp: initializing.
[ 1.319610] misc dsscomp: display0=generic_dpi_panel
[ 1.319610] misc dsscomp: display1=hdmi_panel
[ 1.319610] misc dsscomp: found 2 displays and 4 overlays, WB overlay 1
[ 1.320251] could not allocate slot
[ 1.320709] omap-rproc omap-rproc.1: powering up ipu
[ 1.321136] virtio_rpmsg_bus virtio0: rpmsg backend virtproc probed successfully
[ 1.321624] virtio_rpmsg_bus virtio1: rpmsg backend virtproc probed successfully
[ 1.321624] omap-rproc omap-rproc.0: powering up dsp
[ 1.322174] virtio_rpmsg_bus virtio2: rpmsg backend virtproc probed successfully
[ 1.322174] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 104) is a OMAP UART0
[ 1.323242] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 105) is a OMAP UART1
[ 1.323791] omap_uart.2: ttyO2 at MMIO 0x48020000 (irq = 106) is a OMAP UART2
[ 2.483673] console [ttyO2] enabled
[ 2.487792] omap_uart.3: ttyO3 at MMIO 0x4806e000 (irq = 102) is a OMAP UART3
[ 2.496307] omap_ion_probe: adding heap secure_input of type 2 with aa300000@5a00000
[ 2.504974] omap_ion_probe: adding heap secure_output_wfdhdcp of type 2 with a9300000@800000
[ 2.514312] omap_ion_probe: adding heap tiler of type 4 with a2600000@0
[ 2.521728] omap_ion_probe: adding heap nonsecure_tiler of type 4 with a2600000@0
[ 2.530090] omap_ion_probe: adding heap system of type 0 with 0@0
[ 2.536895] omap_ion_probe: adding heap tiler_reservation of type 5 with 0@0
[ 2.536895] brd: module loaded
[ 2.556854] loop: module loaded
[ 2.563873] PPP generic driver version 2.4.2
[ 2.568817] PPP Deflate Compression module registered
[ 2.574432] PPP BSD Compression module registered
[ 2.580322] PPP MPPE Compression module registered
[ 2.585723] NET: Registered protocol family 24
[ 2.592193] usbcore: registered new interface driver asix
[ 2.598266] usbcore: registered new interface driver cdc_ether
[ 2.601318] usbcore: registered new interface driver smsc95xx
[ 2.611328] usbcore: registered new interface driver net1080
[ 2.613861] usbcore: registered new interface driver cdc_subset
[ 2.621673] usbcore: registered new interface driver zaurus
[ 2.630584] cdc_ncm: 04-Aug-2011
[ 2.630615] usbcore: registered new interface driver cdc_ncm
[ 2.640625] usbcore: registered new interface driver zd1201
[ 2.646942] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.654388] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
[ 2.654388] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
[ 2.669006] ehci-omap ehci-omap.0: irq 109, io mem 0x4a064c00
[ 2.684173] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[ 2.690612] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 2.698181] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.706237] usb usb1: Product: OMAP-EHCI Host Controller
[ 2.712127] usb usb1: Manufacturer: Linux 3.0.31-01923-g519bdcb-dirty ehci_hcd
[ 2.720184] usb usb1: SerialNumber: ehci-omap.0
[ 2.725677] hub 1-0:1.0: USB hub found
[ 2.725677] hub 1-0:1.0: 3 ports detected
[ 2.833435] usbcore: registered new interface driver cdc_acm
[ 2.833435] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 2.833435] Initializing USB Mass Storage driver...
[ 2.854217] usbcore: registered new interface driver usb-storage
[ 2.860931] USB Mass Storage support registered.
[ 2.866210] usbcore: registered new interface driver usbserial
[ 2.872741] usbserial: USB Serial Driver core
[ 2.872772] USB Serial support registered for Keyspan - (without firmware)
[ 2.877655] USB Serial support registered for Keyspan 1 port adapter
[ 2.892364] USB Serial support registered for Keyspan 2 port adapter
[ 2.899536] USB Serial support registered for Keyspan 4 port adapter
[ 2.906707] usbcore: registered new interface driver keyspan
[ 2.912994] keyspan: v1.1.5:Keyspan USB to Serial Converter Driver
[ 2.920257] mousedev: PS/2 mouse device common for all mice
[ 2.927307] twl_rtc twl_rtc: Power up reset detected.
[ 2.933929] twl_rtc twl_rtc: Enabling TWL-RTC.
[ 2.940643] using rtc device, twl_rtc, for alarms
[ 2.940643] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
[ 2.953125] i2c /dev entries driver
[ 2.957092] lirc_dev: IR Remote Control driver registered, major 250
[ 2.964843] IR NEC protocol handler initialized
[ 2.969909] IR RC5(x) protocol handler initialized
[ 2.969909] IR RC6 protocol handler initialized
[ 2.980316] IR JVC protocol handler initialized
[ 2.980316] IR Sony protocol handler initialized
[ 2.990539] IR RC5 (streamzap) protocol handler initialized
[ 2.990539] IR LIRC bridge handler initialized
[ 2.990539] dmm: probe base: fd300000, irq 145
[ 3.009063] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 3.017242] device-mapper: uevent: version 1.0.3
[ 3.022369] device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: dm-devel@redhat.com
[ 3.022369] Bluetooth: HCI UART driver ver 2.2
[ 3.022369] Bluetooth: HCI H4 protocol initialized
[ 3.042419] cpuidle: using governor ladder
[ 3.046997] cpuidle: using governor menu
[ 3.056823] usbcore: registered new interface driver usbhid
[ 3.061492] usb 1-1: new high speed USB device number 2 using ehci-omap
[ 3.070281] usbhid: USB HID core driver
[ 3.074829] logger: created 256K log 'log_main'
[ 3.079803] logger: created 256K log 'log_events'
[ 3.085266] logger: created 256K log 'log_radio'
[ 3.085266] logger: created 256K log 'log_system'
[ 3.096221] thermal_sensor_set_temp: no cooling agents for domain cpu
[ 3.105377] omap_report_temp:thermal_sensor_set_temp reports error
[ 3.112457] omap_temp_sensor omap_temp_sensor.0: omap_ondie_sensor : 'omap_temp_sensor'
[ 3.112457] thermal_sensor_set_temp: no cooling agents for domain cpu
[ 3.112518] OMAPRPC: Registration of OMAPRPC rpmsg service returned 0!
[ 3.141601] SDP4430 SoC init
[ 3.152587] twl6040-codec twl6040-codec: couldn't get VDDHF regulator -19
[ 3.187805] asoc: null-codec-dai <-> MultiMedia1 mapping ok
[ 3.195098] asoc: null-codec-dai <-> MultiMedia2 mapping ok
[ 3.202575] asoc: null-codec-dai <-> Voice mapping ok
[ 3.209136] asoc: null-codec-dai <-> Tones mapping ok
[ 3.215698] asoc: null-codec-dai <-> Vibra mapping ok
[ 3.221954] asoc: null-codec-dai <-> MODEM mapping ok
[ 3.228210] asoc: null-codec-dai <-> MultiMedia1 LP mapping ok
[ 3.235809] asoc: FM Digital <-> omap-mcbsp-dai.1 mapping ok
[ 3.242309] usb 1-1: New USB device found, idVendor=0424, idProduct=9514
[ 3.243133] asoc: twl6040-dl1 <-> mcpdm-dl mapping ok
[ 3.244659] asoc: dmic-hifi <-> omap-dmic-dai-0 mapping ok
[ 3.261169] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 3.269073] twl6040-codec twl6040-codec: ASoC: Failed to create Aux/FM Stereo In debugfs file
[ 3.278594] hub 1-1:1.0: USB hub found
[ 3.279266] asoc: twl6040-dl1 <-> mcpdm-dl1 mapping ok
[ 3.279998] asoc: twl6040-ul <-> mcpdm-ul1 mapping ok
[ 3.280731] asoc: twl6040-dl2 <-> mcpdm-dl2 mapping ok
[ 3.281494] asoc: twl6040-vib <-> mcpdm-vib mapping ok
[ 3.282226] asoc: Bluetooth <-> omap-mcbsp-dai.0 mapping ok
[ 3.282958] asoc: Bluetooth <-> omap-mcbsp-dai.0 mapping ok
[ 3.283752] asoc: FM Digital <-> omap-mcbsp-dai.1 mapping ok
[ 3.284515] asoc: MODEM <-> omap-mcbsp-dai.1 mapping ok
[ 3.285247] asoc: dmic-hifi <-> omap-dmic-abe-dai-0 mapping ok
[ 3.286010] asoc: dmic-hifi <-> omap-dmic-abe-dai-1 mapping ok
[ 3.286743] asoc: dmic-hifi <-> omap-dmic-abe-dai-2 mapping ok
[ 3.287506] asoc: null-codec-dai <-> omap-abe-vxrec-dai mapping ok
[ 3.289276] input: Panda Headset Jack as /devices/platform/soc-audio/sound/card0/input0
[ 3.290924] ALSA device list:
[ 3.290924] #0: TI OMAP4 Board
[ 3.291015] GACT probability NOT on
[ 3.291046] Mirror/redirect action on
[ 3.291046] u32 classifier
[ 3.291046] Actions configured
[ 3.291046] Netfilter messages via NETLINK v0.30.
[ 3.291137] nf_conntrack version 0.5.0 (8170 buckets, 32680 max)
[ 3.291931] ctnetlink v0.93: registering with nfnetlink.
[ 3.292175] xt_time: kernel timezone is -0000
[ 3.293853] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 3.293975] arp_tables: (C) 2002 David S. Miller
[ 3.294067] TCP cubic registered
[ 3.294708] NET: Registered protocol family 10
[ 3.299011] Mobile IPv6
[ 3.299041] IPv6 over IPv4 tunneling driver
[ 3.303436] NET: Registered protocol family 17
[ 3.303466] NET: Registered protocol family 15
[ 3.324890] Bluetooth: RFCOMM TTY layer initialized
[ 3.324920] Bluetooth: RFCOMM socket layer initialized
[ 3.324920] Bluetooth: RFCOMM ver 1.11
[ 3.324951] NET: Registered protocol family 35
[ 3.325317] lib80211: common routines for IEEE802.11 drivers
[ 3.325317] lib80211_crypt: registered algorithm 'NULL'
[ 3.325347] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 3.486236] hub 1-1:1.0: 5 ports detected
[ 3.486236] ThumbEE CPU extension supported.
[ 3.486267] Registering SWP/SWPB emulation handler
[ 3.504516] Reprogramming LPDDR2 timings to 400000000 Hz
[ 3.510559] sr_init: No PMIC hook to init smartreflex
[ 3.516296] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized
[ 3.524963] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized
[ 3.533691] smartreflex smartreflex.2: omap_sr_probe: SmartReflex driver initialized
[ 3.542785] thermal_lookup_temp: pcb is a non existing domain
[ 3.549163] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 3.558074] omap_cpu_thermal_manager:sensor 35600 avg sensor 0 pcb
[ 3.564788] 0, delta 3087 hot spot 38687
[ 3.569488] omap_cpu_thermal_manager: hot spot temp 38687 - going into safe zone
[ 3.577636] thermal_lookup_temp: pcb is a non existing domain
[ 3.584075] mmc0: new high speed SDHC card at address 0007
[ 3.590484] thermal_lookup_temp: pcb is a non existing domain
[ 3.596862] thermal_lookup_temp: pcb is a non existing domain
[ 3.603271] mmcblk0: mmc0:0007 SD16G 14.9 GiB
[ 3.608764] Power Management for TI OMAP4.
[ 3.613494] OMAP4 PM: Static dependency added between MPUSS and DUCATI <-> L4_PER/CFG and L3_1.
[ 3.625213] mmcblk0: p1 p2 p3 p4 < p5 p6 >
[ 3.630554] clock: disabling unused clocks to save power
[ 3.751373] mmc1: card claims to support voltages below the defined range. These will be ignored.
[ 3.787139] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
[ 3.794586] mmc1: new SDIO card at address 0001
[ 3.817108] usb 1-1.1: new high speed USB device number 3 using ehci-omap
[ 3.936218] cannot apply mgr(lcd) on inactive device
[ 3.949859] omapfb omapfb: failed to apply dispc config
[ 3.955718] cannot apply mgr(tv) on inactive device
[ 3.973480] omapfb omapfb: failed to apply dispc config
[ 3.979309] usb 1-1.1: New USB device found, idVendor=0424, idProduct=ec00
[ 3.996734] cannot apply mgr(lcd2) on inactive device
[ 4.002410] omapfb omapfb: failed to apply dispc config
[ 4.008178] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 4.016723] omapdss DPI: Could not find exact pixel clock. Requested 74250 kHz, got 76800 kHz
[ 4.028137] smsc95xx v1.0.4
[ 4.031585] regulator_init_complete: VANA: incomplete constraints, leaving on
[ 4.040496] regulator_init_complete: VDAC: incomplete constraints, leaving on
[ 4.048706] regulator_init_complete: VCXIO: incomplete constraints, leaving on
[ 4.062255] twl_rtc twl_rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801)
[ 4.090423] thermal_lookup_temp: pcb is a non existing domain
[ 4.096740] thermal_lookup_temp: pcb is a non existing domain
[ 4.103027] thermal_lookup_temp: pcb is a non existing domain
[ 4.118011] smsc95xx 1-1.1:1.0: eth0: register 'smsc95xx' at usb-ehci-omap.0-1.1, smsc95xx USB 2.0 Ethernet, 4a:9c:54:55:08:e7
[ 4.215576] usb 1-1.2: new low speed USB device number 4 using ehci-omap
[ 4.355987] usb 1-1.2: New USB device found, idVendor=045e, idProduct=0040
[ 4.363739] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 4.372161] usb 1-1.2: Product: Microsoft Wheel Mouse Optical®
[ 4.378753] usb 1-1.2: Manufacturer: Microsoft
[ 4.393432] input: Microsoft Microsoft Wheel Mouse Optical® as /devices/platform/omap/usbhs_omap/ehci-omap.0/usb1/1-1/1-1.2/1-1.2:1.0/input/input1
[ 4.408843] generic-usb 0003:045E:0040.0001: input: USB HID v1.00 Mouse [Microsoft Microsoft Wheel Mouse Optical®] on usb-ehci-omap.0-1.2/input0
[ 4.504852] usb 1-1.3: new low speed USB device number 5 using ehci-omap
[ 4.635498] usb 1-1.3: New USB device found, idVendor=046d, idProduct=c31c
[ 4.643249] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 4.651611] usb 1-1.3: Product: USB Keyboard
[ 4.656463] usb 1-1.3: Manufacturer: Logitech
[ 4.669616] input: Logitech USB Keyboard as /devices/platform/omap/usbhs_omap/ehci-omap.0/usb1/1-1/1-1.3/1-1.3:1.0/input/input2
[ 4.683013] generic-usb 0003:046D:C31C.0002: input: USB HID v1.10 Keyboard [Logitech USB Keyboard] on usb-ehci-omap.0-1.3/input0
[ 4.705841] input: Logitech USB Keyboard as /devices/platform/omap/usbhs_omap/ehci-omap.0/usb1/1-1/1-1.3/1-1.3:1.1/input/input3
[ 4.719116] generic-usb 0003:046D:C31C.0003: input: USB HID v1.10 Device [Logitech USB Keyboard] on usb-ehci-omap.0-1.3/input1
[ 5.106109] thermal_lookup_temp: pcb is a non existing domain
[ 5.112609] thermal_lookup_temp: pcb is a non existing domain
[ 5.119293] thermal_lookup_temp: pcb is a non existing domain
[ 6.121734] thermal_lookup_temp: pcb is a non existing domain
[ 6.128387] thermal_lookup_temp: pcb is a non existing domain
[ 6.134918] thermal_lookup_temp: pcb is a non existing domain
[ 7.137603] thermal_lookup_temp: pcb is a non existing domain
[ 7.144104] thermal_lookup_temp: pcb is a non existing domain
[ 7.150787] thermal_lookup_temp: pcb is a non existing domain
[ 8.152984] thermal_lookup_temp: pcb is a non existing domain
[ 8.159637] thermal_lookup_temp: pcb is a non existing domain
[ 8.166137] thermal_lookup_temp: pcb is a non existing domain
[ 9.168609] thermal_lookup_temp: pcb is a non existing domain
[ 9.175079] thermal_lookup_temp: pcb is a non existing domain
[ 9.181762] thermal_lookup_temp: pcb is a non existing domain
[ 10.184234] thermal_lookup_temp: pcb is a non existing domain
[ 10.190887] thermal_lookup_temp: pcb is a non existing domain
[ 10.197418] thermal_lookup_temp: pcb is a non existing domain
[ 11.199859] thermal_lookup_temp: pcb is a non existing domain
[ 11.206359] thermal_lookup_temp: pcb is a non existing domain
[ 11.213043] thermal_lookup_temp: pcb is a non existing domain
[ 12.215484] thermal_lookup_temp: pcb is a non existing domain
[ 12.222106] thermal_lookup_temp: pcb is a non existing domain
[ 12.228668] thermal_lookup_temp: pcb is a non existing domain
[ 13.231353] thermal_lookup_temp: pcb is a non existing domain
[ 13.237854] thermal_lookup_temp: pcb is a non existing domain
[ 13.244537] thermal_lookup_temp: pcb is a non existing domain
[ 14.246734] thermal_lookup_temp: pcb is a non existing domain
[ 14.253234] thermal_lookup_temp: pcb is a non existing domain
[ 14.259918] thermal_lookup_temp: pcb is a non existing domain
[ 15.262359] thermal_lookup_temp: pcb is a non existing domain
[ 15.269012] thermal_lookup_temp: pcb is a non existing domain
[ 15.275543] thermal_lookup_temp: pcb is a non existing domain
[ 16.277954] thermal_lookup_temp: pcb is a non existing domain
[ 16.284454] thermal_lookup_temp: pcb is a non existing domain
[ 16.291137] thermal_lookup_temp: pcb is a non existing domain
[ 17.293579] thermal_lookup_temp: pcb is a non existing domain
[ 17.300262] thermal_lookup_temp: pcb is a non existing domain
[ 17.306762] thermal_lookup_temp: pcb is a non existing domain
[ 18.309234] thermal_lookup_temp: pcb is a non existing domain
[ 18.315734] thermal_lookup_temp: pcb is a non existing domain
[ 18.322418] thermal_lookup_temp: pcb is a non existing domain
[ 19.325103] thermal_lookup_temp: pcb is a non existing domain
[ 19.331726] thermal_lookup_temp: pcb is a non existing domain
[ 19.338256] thermal_lookup_temp: pcb is a non existing domain
[ 20.340484] thermal_lookup_temp: pcb is a non existing domain
[ 20.346984] thermal_lookup_temp: pcb is a non existing domain
[ 20.353637] thermal_lookup_temp: pcb is a non existing domain
[ 21.356109] thermal_lookup_temp: pcb is a non existing domain
[ 21.362762] thermal_lookup_temp: pcb is a non existing domain
[ 21.369293] thermal_lookup_temp: pcb is a non existing domain
[ 22.371704] thermal_lookup_temp: pcb is a non existing domain
[ 22.378234] thermal_lookup_temp: pcb is a non existing domain
[ 22.384887] thermal_lookup_temp: pcb is a non existing domain
[ 23.387359] thermal_lookup_temp: pcb is a non existing domain
[ 23.394012] thermal_lookup_temp: pcb is a non existing domain
[ 23.400543] thermal_lookup_temp: pcb is a non existing domain
[ 24.402984] thermal_lookup_temp: pcb is a non existing domain
[ 24.409484] thermal_lookup_temp: pcb is a non existing domain
[ 24.416168] thermal_lookup_temp: pcb is a non existing domain
[ 25.418853] thermal_lookup_temp: pcb is a non existing domain
[ 25.425506] thermal_lookup_temp: pcb is a non existing domain
[ 25.432006] thermal_lookup_temp: pcb is a non existing domain
[ 26.434234] thermal_lookup_temp: pcb is a non existing domain
[ 26.440734] thermal_lookup_temp: pcb is a non existing domain
[ 26.447418] thermal_lookup_temp: pcb is a non existing domain
[ 27.449859] thermal_lookup_temp: pcb is a non existing domain
[ 27.456481] thermal_lookup_temp: pcb is a non existing domain
[ 27.463012] thermal_lookup_temp: pcb is a non existing domain
[ 28.465484] thermal_lookup_temp: pcb is a non existing domain
[ 28.471984] thermal_lookup_temp: pcb is a non existing domain
[ 28.478668] thermal_lookup_temp: pcb is a non existing domain
[ 29.481079] thermal_lookup_temp: pcb is a non existing domain
[ 29.487731] thermal_lookup_temp: pcb is a non existing domain
[ 29.494262] thermal_lookup_temp: pcb is a non existing domain
[ 30.496734] thermal_lookup_temp: pcb is a non existing domain
[ 30.503234] thermal_lookup_temp: pcb is a non existing domain
[ 30.509887] thermal_lookup_temp: pcb is a non existing domain
[ 31.512603] thermal_lookup_temp: pcb is a non existing domain
[ 31.519226] thermal_lookup_temp: pcb is a non existing domain
[ 31.525787] thermal_lookup_temp: pcb is a non existing domain
[ 32.527984] thermal_lookup_temp: pcb is a non existing domain
[ 32.534484] thermal_lookup_temp: pcb is a non existing domain
[ 32.541137] thermal_lookup_temp: pcb is a non existing domain
[ 33.543609] thermal_lookup_temp: pcb is a non existing domain
[ 33.550262] thermal_lookup_temp: pcb is a non existing domain
[ 33.556793] thermal_lookup_temp: pcb is a non existing domain
[ 34.559234] thermal_lookup_temp: pcb is a non existing domain
[ 34.565734] thermal_lookup_temp: pcb is a non existing domain
[ 34.572387] thermal_lookup_temp: pcb is a non existing domain
[ 35.574829] thermal_lookup_temp: pcb is a non existing domain
[ 35.581481] thermal_lookup_temp: pcb is a non existing domain
[ 35.588134] thermal_lookup_temp: pcb is a non existing domain
[ 36.590484] thermal_lookup_temp: pcb is a non existing domain
[ 36.597137] thermal_lookup_temp: pcb is a non existing domain
[ 36.603668] thermal_lookup_temp: pcb is a non existing domain
[ 37.606323] thermal_lookup_temp: pcb is a non existing domain
[ 37.612854] thermal_lookup_temp: pcb is a non existing domain
[ 37.619537] thermal_lookup_temp: pcb is a non existing domain
[ 38.621734] thermal_lookup_temp: pcb is a non existing domain
[ 38.628356] thermal_lookup_temp: pcb is a non existing domain
[ 38.634887] thermal_lookup_temp: pcb is a non existing domain
[ 39.637359] thermal_lookup_temp: pcb is a non existing domain
[ 39.643859] thermal_lookup_temp: pcb is a non existing domain
[ 39.650512] thermal_lookup_temp: pcb is a non existing domain
[ 40.652984] thermal_lookup_temp: pcb is a non existing domain
[ 40.659606] thermal_lookup_temp: pcb is a non existing domain
[ 40.666137] thermal_lookup_temp: pcb is a non existing domain
[ 41.668609] thermal_lookup_temp: pcb is a non existing domain
[ 41.675079] thermal_lookup_temp: pcb is a non existing domain
[ 41.681762] thermal_lookup_temp: pcb is a non existing domain
[ 42.684204] thermal_lookup_temp: pcb is a non existing domain
[ 42.690856] thermal_lookup_temp: pcb is a non existing domain
[ 42.697387] thermal_lookup_temp: pcb is a non existing domain
[ 43.700103] thermal_lookup_temp: pcb is a non existing domain
[ 43.706604] thermal_lookup_temp: pcb is a non existing domain
[ 43.713256] thermal_lookup_temp: pcb is a non existing domain
[ 44.715484] thermal_lookup_temp: pcb is a non existing domain
[ 44.722137] thermal_lookup_temp: pcb is a non existing domain
[ 44.728668] thermal_lookup_temp: pcb is a non existing domain
[ 45.731079] thermal_lookup_temp: pcb is a non existing domain
[ 45.737609] thermal_lookup_temp: pcb is a non existing domain
[ 45.744293] thermal_lookup_temp: pcb is a non existing domain
[ 46.746734] thermal_lookup_temp: pcb is a non existing domain
[ 46.753387] thermal_lookup_temp: pcb is a non existing domain
[ 46.759948] thermal_lookup_temp: pcb is a non existing domain
[ 47.762359] thermal_lookup_temp: pcb is a non existing domain
[ 47.768890] thermal_lookup_temp: pcb is a non existing domain
[ 47.775543] thermal_lookup_temp: pcb is a non existing domain
[ 48.777984] thermal_lookup_temp: pcb is a non existing domain
[ 48.784637] thermal_lookup_temp: pcb is a non existing domain
[ 48.791168] thermal_lookup_temp: pcb is a non existing domain
[ 49.793853] thermal_lookup_temp: pcb is a non existing domain
[ 49.800384] thermal_lookup_temp: pcb is a non existing domain
[ 49.807067] thermal_lookup_temp: pcb is a non existing domain
[ 50.809234] thermal_lookup_temp: pcb is a non existing domain
[ 50.815887] thermal_lookup_temp: pcb is a non existing domain
[ 50.822387] thermal_lookup_temp: pcb is a non existing domain
[ 51.824829] thermal_lookup_temp: pcb is a non existing domain
[ 51.831359] thermal_lookup_temp: pcb is a non existing domain
[ 51.838012] thermal_lookup_temp: pcb is a non existing domain
[ 52.840484] thermal_lookup_temp: pcb is a non existing domain
[ 52.847106] thermal_lookup_temp: pcb is a non existing domain
[ 52.853637] thermal_lookup_temp: pcb is a non existing domain
[ 53.856109] thermal_lookup_temp: pcb is a non existing domain
[ 53.862579] thermal_lookup_temp: pcb is a non existing domain
[ 53.869262] thermal_lookup_temp: pcb is a non existing domain
[ 54.871734] thermal_lookup_temp: pcb is a non existing domain
[ 54.878387] thermal_lookup_temp: pcb is a non existing domain
[ 54.884948] thermal_lookup_temp: pcb is a non existing domain
[ 55.887573] thermal_lookup_temp: pcb is a non existing domain
[ 55.894104] thermal_lookup_temp: pcb is a non existing domain
[ 55.900756] thermal_lookup_temp: pcb is a non existing domain
[ 56.902984] thermal_lookup_temp: pcb is a non existing domain
[ 56.909637] thermal_lookup_temp: pcb is a non existing domain
[ 56.916168] thermal_lookup_temp: pcb is a non existing domain
[ 57.918609] thermal_lookup_temp: pcb is a non existing domain
[ 57.925262] thermal_lookup_temp: pcb is a non existing domain
[ 57.931793] thermal_lookup_temp: pcb is a non existing domain
[ 58.934234] thermal_lookup_temp: pcb is a non existing domain
[ 58.940734] thermal_lookup_temp: pcb is a non existing domain
[ 58.947418] thermal_lookup_temp: pcb is a non existing domain
[ 59.949829] thermal_lookup_temp: pcb is a non existing domain
[ 59.956481] thermal_lookup_temp: pcb is a non existing domain
[ 59.963012] thermal_lookup_temp: pcb is a non existing domain
[ 60.965484] thermal_lookup_temp: pcb is a non existing domain
[ 60.971984] thermal_lookup_temp: pcb is a non existing domain
[ 60.978668] thermal_lookup_temp: pcb is a non existing domain
[ 61.981323] thermal_lookup_temp: pcb is a non existing domain
[ 61.987976] thermal_lookup_temp: pcb is a non existing domain
[ 61.994537] thermal_lookup_temp: pcb is a non existing domain
[ 62.005554] omap-rproc omap-rproc.1: rproc_loader_cont: failed to load ducati-m3.bin
[ 62.014526] omap-rproc omap-rproc.0: rproc_loader_cont: failed to load tesla-dsp.bin
[ 62.997497] thermal_lookup_temp: pcb is a non existing domain
[ 63.004150] thermal_lookup_temp: pcb is a non existing domain
[ 63.010681] thermal_lookup_temp: pcb is a non existing domain
[ 64.013122] thermal_lookup_temp: pcb is a non existing domain
[ 64.019622] thermal_lookup_temp: pcb is a non existing domain
[ 64.026306] thermal_lookup_temp: pcb is a non existing domain
[ 65.028778] thermal_lookup_temp: pcb is a non existing domain
[ 65.035430] thermal_lookup_temp: pcb is a non existing domain
[ 65.041961] thermal_lookup_temp: pcb is a non existing domain
[ 65.130493] wl1271: ERROR could not get nvs file: -2
[ 65.146057] wl1271: loaded
[ 65.149230] wl1271: initialized
[ 65.156433] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities
[ 66.028717] List of all partitions:
[ 66.032928] b300 15634432 mmcblk0 driver: mmcblk
[ 66.039215] b301 135136 mmcblk0p1 00000000-0000-0000-0000-000000000000
[ 66.043640] thermal_lookup_temp: pcb is a non existing domain
[ 66.043670] thermal_lookup_temp: pcb is a non existing domain
[ 66.043670] thermal_lookup_temp: pcb is a non existing domain
[ 66.067504]
[ 66.069335] b302 524288 mmcblk0p2 00000000-0000-0000-0000-000000000000
[ 66.078094] b303 262144 mmcblk0p3 00000000-0000-0000-0000-000000000000
[ 66.086853] b304 1 mmcblk0p4 00000000-0000-0000-0000-000000000000
[ 66.095489] b305 524272 mmcblk0p5 00000000-0000-0000-0000-000000000000
[ 66.104248] b306 14188528 mmcblk0p6 00000000-0000-0000-0000-000000000000
[ 66.113006] No filesystem could mount root, tried: ext3
[ 66.119384] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
[ 66.129028] Backtrace:
[ 66.132141] [<c00511ec>] (dump_backtrace+0x0/0x10c) from [<c050fde8>] (dump_stack+0x18/0x1c)
[ 66.141754] r6:00008000 r5:c063c9f0 r4:c0739348 r3:00000000
[ 66.148925] [<c050fdd0>] (dump_stack+0x0/0x1c) from [<c05102bc>] (panic+0x7c/0x1c0)
[ 66.157714] [<c0510240>] (panic+0x0/0x1c0) from [<c0008e08>] (mount_block_root+0x244/0x294)
[ 66.167266] r3:e0841f24 r2:00000020 r1:e0841f58 r0:c063c9f0
[ 66.174407] r7:c063ca60
[ 66.177612] [<c0008bc4>] (mount_block_root+0x0/0x294) from [<c0008fa0>] (mount_root+0x5c/0x6c)
[ 66.187469] [<c0008f44>] (mount_root+0x0/0x6c) from [<c0009120>] (prepare_namespace+0x170/0x1c4)
[ 66.197509] r5:c0039d7d r4:c07363a0
[ 66.201995] [<c0008fb0>] (prepare_namespace+0x0/0x1c4) from [<c0008a38>] (kernel_init+0x100/0x130)
[ 66.212249] r5:c0039334 r4:c0039334
[ 66.216796] [<c0008938>] (kernel_init+0x0/0x130) from [<c0097d44>] (do_exit+0x0/0x6a8)
[ 66.225860] r5:c0008938 r4:00000000
[ 66.230377] CPU0: stopping
[ 66.233673] Backtrace:
[ 66.236724] [<c00511ec>] (dump_backtrace+0x0/0x10c) from [<c050fde8>] (dump_stack+0x18/0x1c)
[ 66.246337] r6:c0045e80 r5:c06e65a0 r4:00000000 r3:00000000
[ 66.253448] [<c050fdd0>] (dump_stack+0x0/0x1c) from [<c0047444>] (do_IPI+0x164/0x198)
[ 66.262390] [<c00472e0>] (do_IPI+0x0/0x198) from [<c004d008>] (__irq_svc+0x48/0xe0)
[ 66.271118] Exception stack(0xc06d5ed0 to 0xc06d5f18)
[ 66.276855] 5ec0: c06d5f28 c0e8a110 6b5ee72d 0000000f
[ 66.286163] 5ee0: c0e8a100 0000000f c06d5f38 fa241000 c0736c14 c05206c8 00000010 c06d5f6c
[ 66.295349] 5f00: c0e8a100 c06d5f18 00000004 c0065d5c 60000153 ffffffff
[ 66.302978] [<c0065b38>] (omap4_enter_idle+0x0/0x8d0) from [<c033d3f4>] (cpuidle_idle_call+0x94/0x110)
[ 66.313568] [<c033d360>] (cpuidle_idle_call+0x0/0x110) from [<c004e9e0>] (cpu_idle+0xc4/0x100)
[ 66.323364] r6:c0736404 r5:c06ee434 r4:c06d4000 r3:c033d360
[ 66.330474] [<c004e91c>] (cpu_idle+0x0/0x100) from [<c0504f2c>] (rest_init+0x8c/0xa4)
[ 66.339416] r7:c0e87140 r6:c0736340 r5:c06d4000 r4:c06d4000
[ 66.346527] [<c0504ea0>] (rest_init+0x0/0xa4) from [<c00088e4>] (start_kernel+0x2a4/0x2f8)
[ 66.355926] r4:c06e63cc r3:00000000
[ 66.360412] [<c0008640>] (start_kernel+0x0/0x2f8) from [<8000803c>] (0x8000803c)
[ 66.368865] r7:c06ee414 r6:c003a370 r5:c06e62c0 r4:10c5387d
[ 66.375976] Rebooting in 5 seconds..