Other Parts Discussed in Thread: OMAP3530
Hi ,
I'm planning to write an application based on Codec Engine G.711 encode and decode server . So my first step is to copy the "app.c" example in dvsdk_3_00_00_40/codec_engine_2_24/examples/ti/sdo/ce/examples/apps/speech and modified it . Then I write my own config.cfg file and makefile.The application could run without any problem with the function SPHENC1_process( ) commentted, so I think my makefile and config.cfg is correct. When with that function uncommentted there were errors below:
..................
CMEMK Error: get_phys: Unable to find phys addr for 0x0010f044
CMEMK Error: get_phys: get_user_pages() failed: -14
CMEMK Error: GETPHYS: Failed to convert virtual 0x10f044 to physical.
CMEM Error: getPhys: Failed to get physical address of 0x10f044
..................
I googled it and it seems that the address 0x0010f044 is not a virtual address and CMEM could not get its physical address. I have successfully run the loadmodules.sh and the TI's examples could run smoothly.
Then I run it in the debug mode :
#CE_DEBUG=3 ./sphencode
and it said:
========================================================================================================my app
...........
@6,427,917us: [+0 T:0x4001e490 S:0xbef56a04] ti.sdo.ce.speech1.SPHENC1 - SPHENC1_process> Enter (handle=0x4d9d8, inBuf=0xbef56b90, outBuf=0xbef56b84, inArgs=0xbef56b74, outArgs=0xbef56b6c)
@6,428,009us: [+5 T:0x4001e490 S:0xbef569ac] CV - VISA_allocMsg> Allocating message for messageId=0x0002e5c6
@6,428,070us: [+0 T:0x4001e490 S:0xbef5697c] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x40020000, size=64)
@6,428,131us: [+1 T:0x4001e490 S:0xbef5697c] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x40020000, size=64)
@6,428,161us: [+1 T:0x4001e490 S:0xbef5697c] OM - Memory__getPhysicalAddress> found in cb(Sc=0x40020000, Ec=0x40020040, Ss=0x40020000, Es=0x40020040, PSc=0x85ffd000)
@6,428,222us: [+1 T:0x4001e490 S:0xbef5697c] OM - Memory__getPhysicalAddress> returning physAddr=0x85ffd000
@6,428,253us: [+0 T:0x4001e490 S:0xbef5697c] OM - Memory_getBufferPhysicalAddress> return (0x85ffd000)
@6,428,314us: [+0 T:0x4001e490 S:0xbef5697c] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x40021000, size=32)
@6,428,344us: [+1 T:0x4001e490 S:0xbef5697c] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x40021000, size=32)
@6,428,405us: [+1 T:0x4001e490 S:0xbef5697c] OM - Memory__getPhysicalAddress> found in cb(Sc=0x40021000, Ec=0x40021020, Ss=0x40021000, Es=0x40021020, PSc=0x85ffe000)
@6,428,466us: [+1 T:0x4001e490 S:0xbef5697c] OM - Memory_CMEMK Error: get_phys: Unable to find phys addr for 0x0010f044
_getPhysicalAddress> returning pCMEMK Error: get_phys: get_user_pages() failed: -14
hysAddr=0x85ffe000
@6,428,497usCMEMK Error: GETPHYS: Failed to convert virtual 0x10f044 to physical.
: [+0 T:0x4001e490 S:0xbef5697c] OM - Memory_getBufferPhysicalAddress> return (0x85ffe000)
@6,428,558us: [+0 T:0x4001e490 S:0xbef5697c] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x10f044, size=1075085312)
@6,763,641us: [+1 T:0x4001e490 S:0xbef5697c] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x10f044, size=1075085312)
@6,763,702us: [+1 T:0x4001e490 S:0xbef5697c] OM - Memory__getPhysicalAddress> returning physAddr=0x0
CMEM Error: getPhys: Failed to get physical address of 0x10f044
@6,789,428us: [+1 T:0x4001e490 S:0xbef5697c] OM - Memory_getBufferPhysicalAddress> CMEM_getPhys(0x10f044) = 0x0.
@6,789,520us: [+0 T:0x4001e490 S:0xbef5697c] OM - Memory_getBufferPhysicalAddress> return (0x0)
@6,789,581us: [+5 T:0x4001e490 S:0xbef56994] CV - VISA_freeMsg(0x4d9d8, 0x4133e880): Freeing message with messageId=0x0002e5c6
@6,789,642us: [+0 T:0x4001e490 S:0xbef56a04] ti.sdo.ce.speech1.SPHENC1 - SPHENC1_process> Exit (handle=0x4d9d8, retVal=0xffffffff)
.....................
========================================================================================================my app
and the correct print of the Codec Engine's example was below
========================================================================================================TI'example
.......................
Encoder version: 1.00.00.0
App-> Processing frame 0...
@6,955,291us: [+0 T:0x4001d000 S:0xbecc7a14] ti.sdo.ce.speech1.SPHENC1 - SPHENC1_process> Enter (handle=0x5dcf8, inBuf=0xbecc7b98, outBuf=0xbecc7b8c, inArgs=0xbecc7b7c, outArgs=0xbecc7ba4)
@6,955,383us: [+5 T:0x4001d000 S:0xbecc79bc] CV - VISA_allocMsg> Allocating message for messageId=0x0002aa5a
@6,955,444us: [+0 T:0x4001d000 S:0xbecc798c] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x4001e000, size=64)
@6,955,474us: [+1 T:0x4001d000 S:0xbecc798c] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x4001e000, size=64)
@6,955,535us: [+1 T:0x4001d000 S:0xbecc798c] OM - Memory__getPhysicalAddress> found in cb(Sc=0x4001e000, Ec=0x4001e040, Ss=0x4001e000, Es=0x4001e040, PSc=0x85ffd000)
@6,955,596us: [+1 T:0x4001d000 S:0xbecc798c] OM - Memory__getPhysicalAddress> returning physAddr=0x85ffd000
@6,955,627us: [+0 T:0x4001d000 S:0xbecc798c] OM - Memory_getBufferPhysicalAddress> return (0x85ffd000)
@6,955,688us: [+0 T:0x4001d000 S:0xbecc798c] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x4001f000, size=32)
@6,955,749us: [+1 T:0x4001d000 S:0xbecc798c] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x4001f000, size=32)
@6,955,810us: [+1 T:0x4001d000 S:0xbecc798c] OM - Memory__getPhysicalAddress> found in cb(Sc=0x4001f000, Ec=0x4001f020, Ss=0x4001f000, Es=0x4001f020, PSc=0x85ffe000)
@6,955,871us: [+1 T:0x4001d000 S:0xbecc798c] OM - Memory__getPhysicalAddress> returning physAddr=0x85ffe000
@6,955,902us: [+0 T:0x4001d000 S:0xbecc798c] OM - Memory_getBufferPhysicalAddress> return (0x85ffe000)
@6,955,963us: [+0 T:0x4001d000 S:0xbecc79bc] CV - VISA_call(visa=0x5dcf8, msg=0x41164880): messageId=0x0002aa5a, command=0x0
@6,956,024us: [+0 T:0x4001d000 S:0xbecc7984] OC - Comm_put> Enter(queue=0x2, msg=0x41164880)
@6,956,085us: [+0 T:0x4001d000 S:0xbecc7984] OC - Comm_put> return (0)
@6,956,146us: [+0 T:0x4001d000 S:0xbecc797c] OC - Comm_get> Enter(queue=0x10001, msg=0xbecc7a2c, timeout=-1)
@6,963,073us: [+0 T:0x4001d000 S:0xbecc797c] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
@6,963,134us: [+0 T:0x4001d000 S:0xbecc790c] OC - Comm_put> Enter(queue=0x0, msg=0x41163880)
@6,963,226us: [+0 T:0x4001d000 S:0xbecc790c] OC - Comm_put> return (0)
@7,296,813us: [+0 T:0x4001d000 S:0xbecc7904] OC - Comm_get> Enter(queue=0x10000, msg=0xbecc79a4, timeout=-1)
@7,296,905us: [+0 T:0x4001d000 S:0xbecc7904] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
[DSP] @3,958,714tk: [+5 T:0x8783af4c S:0x8783d43c] CN - NODE> 0x8783aa68(g711enc#0) call(algHandle=0x8783ab28, msg=0x87e04880); messageId=0x0002aa5a
[DSP] @3,958,793tk: [+0 T:0x8783af4c S:0x8783d3dc] OM - Memory_cacheInv> Enter(addr=0x85ffd000, sizeInBytes=64)
[DSP] @3,958,852tk: [+0 T:0x8783af4c S:0x8783d3dc] OM - Memory_cacheInv> return
[DSP] @3,958,893tk: [+0 T:0x8783af4c S:0x8783d3dc] OM - Memory_cacheInv> Enter(addr=0x85ffe000, sizeInBytes=32)
[DSP] @3,958,951tk: [+0 T:0x8783af4c S:0x8783d3dc] OM - Memory_cacheInv> return
[DSP] @3,958,994tk: [+0 T:0x8783af4c S:0x8783d39c] ti.sdo.ce.speech1.SPHENC1 - SPHENC1_process> Enter (handle=0x8783ab28, inBuf=0x8783d444, outBuf=0x8783d450, inArgs=0x87e048c8, outArgs=0x87e048d8)
[DSP] @3,959,097tk: [+5 T:0x8783af4c S:0x8783d37c] CV - VISA_enter(visa=0x8783ab28): algHandle = 0x8783ab58
[DSP] @3,959,155tk: [+0 T:0x8783af4c S:0x8783d35c] ti.sdo.ce.alg.Algorithm - Algorithm_activate> Enter(alg=0x8783ab58)
[DSP] @3,959,214tk: [+0 T:0x8783af4c S:0x8783d35c] ti.sdo.ce.alg.Algorithm - Algorithm_activate> Exit
[DSP] @3,959,289tk: [+5 T:0x8783af4c S:0x8783d37c] CV - VISA_exit(visa=0x8783ab28): algHandle = 0x8783ab58
[DSP] @3,959,353tk: [+0 T:0x8783af4c S:0x8783d35c] ti.sdo.ce.alg.Algorithm - Algorithm_deactivate> Enter(alg=0x8783ab58)
[DSP] @3,959,413tk: [+0 T:0x8783af4c S:0x8783d35c] ti.sdo.ce.alg.Algorithm - Algorithm_deactivate> Exit
[DSP] @3,959,465tk: [+0 T:0x8783af4c S:0x8783d39c] ti.sdo.ce.speech1.SPHENC1 - SPHENC1_process> Exit (handle=0x8783ab28, retVal=0x0)
[DSP] @3,959,531tk: [+0 T:0x8783af4c S:0x8783d3dc] OM - Memory_cacheWb> Enter(addr=0x85ffe000, sizeInBytes=32)
[DSP] @3,959,590tk: [+0 T:0x8783af4c S:0x8783d3dc] OM - Memory_cacheWb> return
[DSP] @3,959,633tk: [+5 T:0x8783af4c S:0x8783d43c] CN - NODE> returned from call(algHandle=0x8783ab28, msg=0x87e04880); messageId=0x0002aa5a
[DSP] @3,968,728tk: [+0 T:0x87838f8c S:0x87839f4c] CR - processRmsCmd(0x87e038a8, 4056): cmd = 5
[DSP] @3,968,782tk: [+0 T:0x87838f8c S:0x87839f4c] CR - remote time = 0x0, trace buffer size = 4032
@7,299,957us: [+0 T:0x4001d000 S:0xbecc793c] CE - Engine_fwriteTrace> returning count [2053]
@7,300,018us: [+0 T:0x4001d000 S:0xbecc79bc] CV - VISA_call Completed: messageId=0x0002aa5a, command=0x0, return(status=0)
@7,300,079us: [+5 T:0x4001d000 S:0xbecc79c4] CV - VISA_freeMsg(0x5dcf8, 0x41164880): Freeing message with messageId=0x0002aa5a
@7,300,140us: [+0 T:0x4001d000 S:0xbecc7a14] ti.sdo.ce.speech1.SPHENC1 - SPHENC1_process> Exit (handle=0x5dcf8, retVal=0x0)
......................
========================================================================================================TI's example
My application entered virtAddr=0x10f044 and the error occured. Here is my C code:
========================================================================================================my code
#include <xdc/std.h>
#include <ti/sdo/ce/Engine.h>
#include <ti/sdo/ce/CERuntime.h>
#include <ti/sdo/ce/speech1/sphenc1.h>
#include <ti/sdo/ce/osal/Memory.h>
#include <ti/sdo/ce/trace/gt.h>
#include <ti/xdais/xdas.h>
#include <stdio.h>
#include <stdlib.h>
#define NSAMPLES 32
#define IFRAMESIZE (NSAMPLES * sizeof(Int16)) /* raw frame (input) */
#define OFRAMESIZE (NSAMPLES * sizeof(Int8)) /* encoded frame (output) */
#ifndef BUFALIGN
#define BUFALIGN Memory_DEFAULTALIGNMENT
#endif
#define MAXVERSIONSIZE 128
static XDAS_Int8 *inBuf;
static XDAS_Int8 *outBuf;
static XDAS_Int8 *versionBuf; /* acquire optional version from codec */
static Void encode(SPHENC1_Handle enc, FILE *in, FILE *out);
int main(int argc, char *argv[])
{
Engine_Handle ce = NULL;
SPHENC1_Handle enc = NULL;
String inFile, outFile;
Engine_Error err;
Int numAlgs;
Engine_AlgInfo algInfo;
FILE *in = NULL;
FILE *out = NULL;
CERuntime_init();
inBuf = (XDAS_Int8 *) Memory_contigAlloc(IFRAMESIZE, BUFALIGN);
if(inBuf!=NULL) printf("inbuf address: %x\n",inBuf);
outBuf = (XDAS_Int8 *)Memory_contigAlloc(OFRAMESIZE, BUFALIGN);
if(outBuf!=NULL) printf("outbuf address: %x\n",outBuf);
versionBuf = (XDAS_Int8 *)Memory_contigAlloc(MAXVERSIONSIZE, BUFALIGN);
if(versionBuf!=NULL) printf("versionBuf address: %x\n",versionBuf);
if(inBuf!=NULL)
printf("memory allocate success\n");
printf("app running\n");
if (argc <= 1) {
inFile = "./in.dat";
outFile = "./out.dat";
}
else if (argc != 3) {
//fprintf(stderr, usage, argv[0]);
exit(1);
}
else {
inFile = argv[1];
outFile = argv[2];
}
ce = Engine_open("sph", NULL, NULL);
if (ce == NULL) {
printf("Error: could not open engine sphenc1 Error code %d.\n", err);
}
enc = SPHENC1_create(ce, "g711enc", NULL);
if (enc != NULL) {
printf("codec open success\n");
}
err = Engine_getNumAlgs("sph", &numAlgs);
if(Engine_EOK==err)
printf("engine getNumAlg succuss\n");
/* open file streams for input and output */
if ((in = fopen(inFile, "rb")) == NULL) {
printf("App-> ERROR: can't read file %s\n", inFile);
}
if ((out = fopen(outFile, "wb")) == NULL) {
printf("App-> ERROR: can't write to file %s\n", outFile);
}
XDM1_SingleBufDesc inBufDesc;
XDM1_SingleBufDesc outBufDesc;
SPHENC1_InArgs encInArgs;
SPHENC1_OutArgs encOutArgs;
encInArgs.size = sizeof(encInArgs);
encOutArgs.size = sizeof(encOutArgs);
inBufDesc.bufSize = NSAMPLES * sizeof(short);
outBufDesc.bufSize = NSAMPLES * sizeof(char);
Int32 status;
if(1== fread(inBuf, IFRAMESIZE, 1, in) ) printf("read from file success!!!\n");
inBufDesc.buf = inBuf;
outBufDesc.buf = outBuf;
status =SPHENC1_process(enc, &inBufDesc, &outBufDesc, &encInArgs,&encOutArgs);
if (status == SPHENC1_EOK)
printf("App-> Encoder frame successful!\n");
if (inBuf) {
Memory_contigFree(inBuf, IFRAMESIZE);
}
if (outBuf) {
Memory_contigFree(outBuf, OFRAMESIZE);
}
if (versionBuf) {
Memory_contigFree(versionBuf, MAXVERSIONSIZE);
}
if (enc) {
SPHENC1_delete(enc);
}
Engine_close(ce);
return 0;
}
========================================================================================================my code
and below is the error print: in the terminal
========================================================================================================
inbuf address: 4001c000
outbuf address: 40021000
versionBuf address: 40b2d000
memory allocate success
app running
codec open success
engine getNumAlg succuss
sphenc1 control success!!!!!!
read from file success!!!
CMEMK Error: get_phys: Unable to find phys addr for 0x0010f044
CMEMK Error: get_phys: get_user_pages() failed: -14
CMEMK Error: GETPHYS: Failed to convert virtual 0x10f044 to physical.
CMEM Error: getPhys: Failed to get physical address of 0x10f044
========================================================================================================
My makefile
========================================================================================================
-include ./Rules.make
XDC_PATH = $(CODEC_INSTALL_DIR)/packages;$(FC_INSTALL_DIR)/packages;$(CE_INSTALL_DIR)/packages;$(LINK_INSTALL_DIR)/packages;$(XDAIS_INSTALL_DIR)/packages;$(CMEM_INSTALL_DIR)/packages;/$(LINUXLIBS_INSTALL_DIR)/include;$(LPM_INSTALL_DIR)/packages;$(BIOS_INSTALL_DIR)/packages;$(BIOSUTILS_INSTALL_DIR)/packages;
CSTOOL_DIR=/home/FC/CodeSourcery/Sourcery_G++_Lite
XDC_INSTALL_DIR = /home/FC/dsprogram/xdctools_3_15_00_50/packages
INCLUDES += -I $(LINUXKERNEL_INSTALL_DIR)/include -I $(BIOS_INSTALL_DIR)/packages/ti/bios/include -I $(XDAIS_INSTALL_DIR)/packages/ti/xdais/include
LD_LIBS = -lpthread $(LINUXLIBS_INSTALL_DIR)/lib/libasound.so.2 $(LINUXLIBS_INSTALL_DIR)/lib/libncurses.so $(EDITLINE_LIB)
C_FLAGS += -Wall -fno-strict-aliasing -g -I./libedit -DREADLINE=1
CC = $(CSTOOL_PREFIX)gcc $(INCLUDES) $(C_FLAGS) $(shell cat $(XDC_COMPILER_FILE)) -c
AR = $(CSTOOL_PREFIX)ar
LN = $(CSTOOL_PREFIX)gcc
XDC_INSTALL_DIR=/home/FC/dsprogram/xdctools_3_15_00_50
XDCTARGET = gnu.targets.arm.GCArmv5T
XDCPLATFORM = ti.platforms.evm3530
XDC_COMPILER_FILE = $(CONFIGPKG)/compiler.opt
XDC_LINKER_FILE = $(CONFIGPKG)/linker.cmd
CONFIGPKG = sph
CONFIGURO = XDCPATH="$(XDC_PATH)" $(XDC_INSTALL_DIR)/xs xdc.tools.configuro
CONFIG_BLD := config.bld
all:compiler.opt sphencode
compiler.opt:sph.cfg
$(CONFIGURO) -c $(CSTOOL_DIR) \
-t $(XDCTARGET) -p $(XDCPLATFORM) -o $(CONFIGPKG) \
-b $(CONFIG_BLD) $(CONFIGPKG).cfg
sphencode: sphencode.o $(CONFIGPKG)/linker.cmd
$(LN) -o $@ $^ $(LD_LIBS)
%.o:%.c $(XDC_COMPILER_FILE)
$(CC) $(CFLAGS) $(XDC_INCLUDES) -o $@ $<
========================================================================================================
That's all. I have worked on this problem for a long time. Please help, thanks !