This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to open rtsp from DM355IPNC on Linux RHEL?



Hi all.

I have to do this via VLC player. It was compiled with following options:

libvlc was configured with ./configure  '--enable-realrtsp' '--enable-live555' '--with-live555-tree=/usr/src/live' '--disable-nls' '--disable-mozilla' '--enable-shout' '--disable-avcodec' '--disable-avformat' '--disable-swscale' '--disable-postproc' '--enable-debug' '--enable-run-as-root'

When I try to open rtsp from camera, I give errors:

[user@localhost vlc-0.9.9a]$ vlc
VLC media player 0.9.9a Grishenko
[00000001] main libvlc debug: VLC media player - version 0.9.9a Grishenko - (c) 1996-2009 the VideoLAN team
[00000001] main libvlc debug: libvlc was configured with ./configure  '--enable-realrtsp' '--enable-live555' '--with-live555-tree=/usr/src/live' '--disable-nls' '--disable-mozilla' '--enable-shout' '--disable-avcodec' '--disable-avformat' '--disable-swscale' '--disable-postproc'
[00000001] main libvlc debug: translation test: code is "C"
[00000001] main libvlc: Running vlc with the default interface. Use 'cvlc' to use vlc without interface.
[00000334] main interface error: option rtsp-caching does not exist
[00000335] main input error: open of `rtsp://192.168.1.168/mpeg4' failed: could not create access

How to make VLC with support rtsp? Maybe everyone can send me binary? My e-mail is department30 (@) niitv.ru