Other Parts Discussed in Thread: SYSBIOS
Events example:
1) How these functions are using arguments as directly i have not seen any use in the function.
2) Can we pass Void to tak function
3) In this line
tskParams.arg0 = (UArg) mbx;
How we are using argument (tskParams.arg0) inside the function.
Thanks
Code:
#include <xdc/std.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Event.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/knl/Mailbox.h>
#include <xdc/cfg/global.h>
#define NUMMSGS 3 /* number of messages */
#define TIMEOUT 12 /* timeout value */
typedef struct MsgObj {
Int id; /* writer task id */
Char val; /* message value */
} MsgObj, *Msg;
Clock_Handle clk1, clk2;
Event_Handle evt;
Mailbox_Handle mbx;
Semaphore_Handle sem;
Void clk0Fxn(UArg arg0);
Void clk1Fxn(UArg arg0);
Void reader(UArg arg0, UArg arg1);
Void writer(UArg arg0, UArg arg1);
/*
* ======== main ========
*/
Int main()
{
Clock_Params clkParams;
Task_Params tskParams;
Mailbox_Params mbxParams;
Semaphore_Params semParams;
/* Create a one-shot Clock Instance with timeout = 5 system time units */
Clock_Params_init(&clkParams);
clkParams.startFlag = TRUE;
clk1 = Clock_create(clk0Fxn, 5, &clkParams, NULL);
/* Create an one-shot Clock Instance with timeout = 10 system time units */
Clock_Params_init(&clkParams);
clkParams.startFlag = TRUE;
clk2 = Clock_create(clk1Fxn, 10, &clkParams, NULL);
/* create an Event Instance */
evt = Event_create(NULL, NULL);
/* create a Semaphore Instance */
Semaphore_Params_init(&semParams);
semParams.mode = Semaphore_Mode_BINARY;
semParams.event = evt;
semParams.eventId = Event_Id_01;
sem = Semaphore_create(0, &semParams, NULL);
/* create a Mailbox Instance */
Mailbox_Params_init(&mbxParams);
mbxParams.readerEvent = evt;
mbxParams.readerEventId = Event_Id_02;
mbx = Mailbox_create(sizeof(MsgObj), 2, &mbxParams, NULL);
/* create a writer task */
Task_Params_init(&tskParams);
tskParams.priority = 1;
tskParams.arg0 = (UArg) mbx;
Task_create(writer, &tskParams, NULL);
/* create a reader task */
Task_create(reader, &tskParams, NULL);
BIOS_start(); /* does not return */
return(0);
}
/*
* ======== clk0Fxn =======
*/
//Void clk0Fxn(UArg arg0)
Void clk0Fxn(UArg arg0)
{
/* Explicit posting of Event_Id_00 by calling Event_post() */
// Event_post(evt, Event_Id_00);
}
/*
* ======== clk1Fxn =======
*/
Void clk1Fxn(UArg arg0)
{
/* Implicit posting of Event_Id_01 by Sempahore_post() */
// Semaphore_post(sem);
}
/*
* ======== reader ========
*/
Void reader(UArg arg0, UArg arg1)
{
MsgObj msg;
UInt posted;
for (;;) {
/* wait for (Event_Id_00 & Event_Id_01) | Event_Id_02 */
posted = Event_pend(evt,
Event_Id_00 + Event_Id_01, /* andMask */
Event_Id_02, /* orMask */
TIMEOUT);
if (posted == 0) {
System_printf("Timeout expired for Event_pend()\n");
break;
}
if ((posted & Event_Id_00) && (posted & Event_Id_01)) {
if (Semaphore_pend(sem, BIOS_NO_WAIT)) {
System_printf("Explicit posting of Event_Id_00 and Implicit posting of Event_Id_01\n");
}
else {
System_printf("Semaphore not available. Test failed!\n");
}
break;
}
else if (posted & Event_Id_02) {
System_printf("Implicit posting of Event_Id_02\n");
if (Mailbox_pend(mbx, &msg, BIOS_NO_WAIT)) {
/* print value */
System_printf("read id = %d and val = '%c'.\n",msg.id, msg.val);
}
else {
System_printf("Mailbox not available. Test failed!\n");
}
}
else {
System_printf("Unknown Event\n");
break;
}
}
BIOS_exit(0);
}
/*
* ======== writer ========
*/
Void writer(UArg arg0, UArg arg1)
{
MsgObj msg;
Int i;
for (i=0; i < NUMMSGS; i++) {
/* fill in value */
msg.id = i;
msg.val = i + 'a';
System_printf("writing message id = %d val = '%c' ...\n",
msg.id, msg.val);
/* enqueue message */
Mailbox_post(mbx, &msg, TIMEOUT);
}
System_printf("writer done.\n");
}