This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PLLCOUNT problem on TMS320C5402

I'm having some trouble on configuring my DSP C5402 to operate at 100 MHz, through the CLKMD register. The PLLCOUNT bits are calculated through the formula and the graph present in the image below.

However, in this graph from the 320C54x family, there is no 'lockup time' for a CLOCKOUT of 100 MHz. But the C5402 CAN operate at 100 MHz. Pretty weird, huh?

Wich values of 'lockup time' and PLLCOUNT should I choose?

 

Formula and graph: http://img707.imageshack.us/img707/4555/lockup.jpg

 

Thanks,

 

Raphael