Hi,
I'm using OMAP5432 board for my project. I'm facing an issue that I'm unable to add cache memory in my config file. When I try to add I'll get an error message "Unicahe not supported on device". I've seen a similar thread in forum. The solution given was to add device table entry for 5430 in hal/unicahe/cache.xs ,but that didn't solve my problem. I need to enable cache as it seems to have a huge performance hit.
Thanks in advance
Thushara.