Hello All,
I have noticed there are 2 types of HDMI monitors/settings. 1st one is TV screens and 2nd one is PC monitor. Why there is difference?
We are using DM8148 and we need to support most of the formats, 1080i60, 1080i50, 720p60 720p50 etc...
Every resolution works fine with "TV screens" even 1080i50, although I need to change the image format to underscan in the TV othervise it doesn't it to screen.
However I have tried 2 different " PC monitors" and 1080i50 doesn't work. I don't think the monitor doesn't just support that resolution. I beileve there is a setting that I am missing. Do you have any ideas.
My second question is how can I make sure that change the scanning so it will fit to screen when I connect to the "TV Monitor" so I don't need to chage the format of the image all the time.
I am using EZSDK 5_05_02_00 . I have updated the latest HDMI updates in the git repo.
Thank you in advance,
Best Regards,
Hazar