This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Dual Gigabit Ethernet



I have seen some confusing comments in regards to the AM335x devices with the Dual Gigabit Ethernet.. Is there in deed 2 separate RGMII MAC interfaces to the outside world? Can both Ethernet ports run at 1Gbps rate? Customer wants to use as a routing device..What limitations are there in running Gigabit Ethernet in one port and switching out thru the other port? I thought a previous post suggested that only 1 port could be 1Gbps and the other would be 100Mbps? Is that correct?