Dear Sir/Madam,
I am developing a custom board of C6748, booting up via 16-bit NAND flash. I would like to use "AISgen" to generate the AIS output file of my project. Then, write the file to NAND flash by "sfh_OMAP-L138.exe". My project is tested successfully in C6748 LCDK development kit.
I would like to ask if the external DDR2 memory is necessary for my hardware design.
If no external memory is used in my board, could I still boot up my board via 16-bit NAND flash as in C6748 LCDK?
Thank you so much and look forward to your reply.
Best Regards,
Ada