Other Parts Discussed in Thread: SN65HVS882
Hello!
I want to put an digital input to my ICE board, but it doesn't work
I work with the ethercat simple example and I try to read an input and set it to the output LEDs.
Therefore I just connected the 5V output to a switch and this to my first input pin.
5V should work, because the datasheet of the INDUSTRIAL 8-DIGITAL-INPUT SERIALIZER (SN65HVS882) to which the inputs are connected sets the threashold level to 4 - 5.5V.
Does anyone see my fault?
Or any other help?