This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

swms startX/startY parameters set



hi all .when i set the swms layout parameters,i found that 

vdMosaicParam->winList[winId].start_X+1

vdMosaicParam->winList[winId].start_Y+1

above 2 operator result is different .

the startX change 1 pixel is different spacing with the startY change 1 pixcel 

about the spacing of startX+1 is 8 pixel,the spacing of startY+1 is 1pixel

so why? and where can configure that?