This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C clock in EZSDK

Hello,


EZSDK's Linux for DM8168 registers i2c busses to work at 100 kHz in board-support/linux-2.6.37-psp04.04.00.01/arch/arm/mach-omap2/board-ti8168evm.c

But DM8168 I2C controller supports operation at 400 kHz, and all I2C peripherals on the EVM seem to support 400 kHz as well.

Is this a leftover from early versions of EZSDK, or is it set intentionally to 100 kHz to prevent potential problems with custom peripherals which can be connected to EVM via expansion connectors?

Thanks!