All:
There are 2 places to set up stack and heap when using DSP/BIOS - in the .tcf file and in the build settings under the linker.
1. Is it important to make sure that they match?
2. If one forgets to change both places, which setting would take precedence?
This is more of a generic question, but for the record, I am using C6713, DSP/BIOS 5.42, CGT 7.4.4