Other Parts Discussed in Thread: AM3352
Reading the documentation on the EDMA peripheral for this part (am3352), it is clearly capable of doing continuous/chaining DMA transfers via the link-address mechanism. The only method I see that interacts with this mechanism is the "CYCLIC" type transfer, which appears to set the address for the next transfer to the address of the current transfer.
I'd like to set up the DMA for chaining, with four buffers--two for transmit and two for receive, with the following behavior.
T_BUFF_1--currently in use
T_BUFF_2-address is loaded into link register of current transmit operation so that it is automatically utilized when the transfer from T_BUFF_1 completes.
R_BUFF_1-currently in use
R_BUFF_2-address is loaded into link register of current receive operation so that it is automatically utilized when the transfer into R_BUFF_1 completes.
Callback routines associated with these would just load the link-address associated with the new transfer with the address of the buffer not currently in use (the one having just finished).
So the transfers would look like T_BUFF_1 --> T_BUFF_2 --> T_BUFF_1 --> T_BUFF_2 -->.... and R_BUFF_1 --> R_BUFF_2 --> R_BUFF_1 --> R_BUFF_2 -->...
I don't see any full implementations of this in any example/sample code, and like I said, the "CYCLIC" transfers just seem to overwrite the same buffer, rather than update to a new buffer upon completion.
I am writing a replacement for the Linux 3.8 SPI driver ( "spi-omap2-mcspi.c" ) that does continuous transfers rather than the discreet message-queue method, in order to avoid the latency between handling of messages.