Hi, all,i'm working in DVR_RDK 4.0,I want to increase the system tiler size.The DDR size is 2G and mem size is 512,total tiler size is 384 MB.
Can I increase the tiler size ? The config file said it must be aligned on 128MB boundary. I want to modify the file TILER.cfg. I modify UTILS_TILER_CNT_8BIT_SIZE from 128MB to 256MB, and UTILS_TILER_CNT_16BIT_SIZE from (tilerMemSection.len -128MB) to (tilerMemSection.len -256MB), , I can run the program, but the color of video image is wrong
anyone can help me?
Many thanks.