This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FFTC

Hello,

I'm trying to run the FFTC example fftcSimpleK2KC66BiosTestProject, however it hangs at Ipc_start().

This example I imported using the explorer from CCS (v 5.5.0.00077), and it builds correctly.

Do I need to make any configuration in order to run the example?

Michael

  • The output from console is:

    *************** FFTC Testing Start ***************
    **************************************************
    Using FFTC Driver version: 0x2000005 Version Info: FFTC Driver Revision: 02.00.00.05:Dec  4 2013:10:59:04
    Core 0 : L1D cache size 7. L2 cache size 0.

    I forgot to mention, in RTSC the following modules are selected:

    XDCtools – 3.25.3.72

    EDMA3 Low Level Driver – 2.11.9

    Inter-processor Communication – 3.0.2.26

    Keystone2 PDK – 3.0.1.12

    SA LLD – 2.0.1.04

    SYS/BIOS – 6.35.4.50

    Other repository – c:/ti/ccsv5/ccs_base

  • Same case with me!! Following the thread.