Other Parts Discussed in Thread: TPS65217, AM3352
Hello Everyone,
I'm using AM3352 with TPS65217 and would like to know if anyone has tried to run RTC-only while working with Linux. I would like to use the internal RTC, provided with an external 32 KHz crystal and a 1.8V supercap.
I'm using Rev 2.0 or higher silicon, so I'm guessing there are no additional errata's regarding RTC only mode. I also understand that the current consumption of the RTC module is around 30uA at 1.8V (got that from the wiki site).
Do I need to put the RTC in Idle mode to allow it to continue working even if rest of the system is not powered (The datasheet says that the RTC is default in smart-idle mode) ? If so, how to do the same?
Thank you for your replies.
- Santhosh