This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tvp5147m1 composite video capture problem in DM6467

Other Parts Discussed in Thread: TVP5147M1

Hello:

    I have a quesion about vpif capture .

    We have DM6467 custom board that use tvp5147m1 video decoder for composite SDTV input(PAL)。

    tvp5147m1 output mode is BT.656 and connect to vpif channel 0. ALL configs is as follow:

   

vpif
VPIF_CH0_CTRL 000010a9

vpif_channel_config_params=
{
	{
		"PAL_BDGHIK", 720, 576, 25, 0, 1, 280, 1440, 1, 23, 311, 313,
		336, 624, 625, 0, 1, 0, V4L2_STD_625_50,
	},
}

tvp514x m1
tvp514x 1-005d: Reg(0x00): 0x05
tvp514x 1-005d: Reg(0x01): 0x0F
tvp514x 1-005d: Reg(0x02): 0x02
tvp514x 1-005d: Reg(0x03): 0x00
tvp514x 1-005d: Reg(0x05): 0x10
tvp514x 1-005d: Reg(0x06): 0x00
tvp514x 1-005d: Reg(0x07): 0x00
tvp514x 1-005d: Reg(0x08): 0x00
tvp514x 1-005d: Reg(0x09): 0x80
tvp514x 1-005d: Reg(0x0A): 0x80
tvp514x 1-005d: Reg(0x0B): 0x80
tvp514x 1-005d: Reg(0x0C): 0x00
tvp514x 1-005d: Reg(0x0D): 0x00
tvp514x 1-005d: Reg(0x0E): 0x04
tvp514x 1-005d: Reg(0x10): 0x80
tvp514x 1-005d: Reg(0x11): 0x80
tvp514x 1-005d: Reg(0x12): 0x80
tvp514x 1-005d: Reg(0x14): 0x80
tvp514x 1-005d: Reg(0x16): 0x5F
tvp514x 1-005d: Reg(0x17): 0x00
tvp514x 1-005d: Reg(0x18): 0x2F
tvp514x 1-005d: Reg(0x19): 0x03
tvp514x 1-005d: Reg(0x1A): 0x07
tvp514x 1-005d: Reg(0x1B): 0x00
tvp514x 1-005d: Reg(0x1C): 0x47
tvp514x 1-005d: Reg(0x1D): 0x00
tvp514x 1-005d: Reg(0x1E): 0x01
tvp514x 1-005d: Reg(0x1F): 0x00
tvp514x 1-005d: Reg(0x20): 0x04
tvp514x 1-005d: Reg(0x21): 0x00
tvp514x 1-005d: Reg(0x22): 0x6F
tvp514x 1-005d: Reg(0x23): 0x02
tvp514x 1-005d: Reg(0x24): 0x18
tvp514x 1-005d: Reg(0x25): 0x00
tvp514x 1-005d: Reg(0x32): 0x0C
tvp514x 1-005d: Reg(0x33): 0x00
tvp514x 1-005d: Reg(0x34): 0x11
tvp514x 1-005d: Reg(0x35): 0xEE
tvp514x 1-005d: Reg(0x36): 0xAF
tvp514x 1-005d: Reg(0x37): 0xFF
tvp514x 1-005d: Reg(0x38): 0xFF
tvp514x 1-005d: Reg(0x39): 0x01


    however, when we capture a frame like this 

which actually is

can anyone give me some help? thanks!