Other Parts Discussed in Thread: OMAP-L138, SYSBIOS
I am using OMAP-L138 EVM with CCS4 trying to evaluate DSP/BIOS 6 on the DSP core and Linux on the ARM core. I am using the builtin XDS100 for debugging. I don't have any issues w/ the Linux side, but the BIOS timing seems way off. I wrote a basic "blinky" app in a BIOS task to blink the LEDS. I set a certain pattern, use the Task_sleep() function, then update the pattern. The trouble is that everything is SLOW. I have the tick configured to be 1000 us, so Task_sleep(1000) should be a 1 s delay but instead it's ~ 130 s. Task_sleep(10) should be 10 ms but it's > 1 s. The really crazy thing is that if I type in commands to the ARM core running Linux through the serial port it speeds up considerably! I can see the 1 s blink pattern go noticeably faster. I've tried changing the DSP/BIOS configuration ti.sysbios.knl.Clock.timerID (default is -1, I've tried 0, 1, and 2 with no change). I also tried changing the ti.sysbios.knl.Clock.tickPeriod (default is 1000 us, I tried 10) and saw no difference. Where the heck is the tick coming from? I have ti.sysbios.knl.Clock.tickSource set to the default, TickSource_TIMER.