Other Parts Discussed in Thread: OMAP3530
I'm just starting out with the OMAP35XEVM.
I'm trying to boot a Windows CE image from SD w/ KITL. When I try to configure the Ethernet chip, it says there is an "Invalid Ethernet chip ID (0x0)!".
I suspect it's not actually reading from the LAN9220 chip correctly...
Here is the serial output I get:
|
Texas Instruments Windows CE SD X-Loader for EVM 3530 Microsoft Windows CE Bootloader Common Library Version 1.4 Built Dec 10 2009 18: Texas Instruments Windows CE EBOOT for Mistral OMAP EVM, Built Dec 11 2009 at 09 TI OMAP3530 Version 0x4b7ae02f (ES3.1) >>> Forcing cold boot (non-persistent registry and other data will be wiped) <<< Hit space to enter configuration menu 5... -------------------------------------------------------------------------------- Selection: 3 -------------------------------------------------------------------------------- Selection (actual (NULL)): 1 -------------------------------------------------------------------------------- Selection: 4 -------------------------------------------------------------------------------- Selection: 1 Network: |