This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x wince7 compile errors

I am using BSP_WINCE_ARM_A8_02_30_00 on AM335x Wince7 platform.

When I compile am335x wince7 bsp there are

BUILD: [00:0000005056:PROGC ] Building COMPILE Pass in C:\WINCE700\platform\common\src\soc\COMMON_TI_V1\AM389X\Emac\ directory.
BUILD: [01:0000005068:PROGC ] Compiling .\Am389xEmac.c
BUILD: [01:0000005071:ERRORE] Error(s) in directory "C:\WINCE700\platform\common\src\soc\COMMON_TI_V1\AM389X\Emac\". {log="C:\WINCE700\build.log(34688)"}
BUILD: [01:0000005072:ERRORE] c:\wince700\platform\common\src\soc\common_ti_v1\am389x\inc\am389xemacregs.h : error C2220: warning treated as error - no 'object' file generated {log="C:\WINCE700\build.log(34689)"}
BUILD: [01:0000005073:WARNN ] Warning(s) in directory "C:\WINCE700\platform\common\src\soc\COMMON_TI_V1\AM389X\Emac\". {log="C:\WINCE700\build.log(34690)"}
BUILD: [01:0000005074:WARNN ] c:\wince700\platform\common\src\soc\common_ti_v1\am389x\inc\am389xemacregs.h : warning C4819: The file contains a character that cannot be represented in the current code page (936). Save the file in Unicode format to prevent data loss {log="C:\WINCE700\build.log(34691)"}
BUILD: [01:0000005075:ERRORE] NMAKE : fatal error U1077: 'C:\WINCE700\sdk\bin\i386\ARM\cl.EXE' : return code '0x2' {log="C:\WINCE700\build.log(34692)"}
BUILD: [01:0000005077:ERRORE] clean TargetCompilePass -nologo BUILDMSG=Stop. BUILDROOT=C:\WINCE700\platform\common CLEANBUILD=1 NOLINK=1 NOPASS0=1 failed - rc = 2 {log="C:\WINCE700\build.log(34694)"}

errors: