Hi,
We are working on C6746 and CCSv5.2 with SYS-BIOS.
my quiry is "interrupt number" field when we are creating HWI through .cfg file, it can be any number between INT4-15..is it correct or not.
we are assigned UART2 HWI interrupt number as 9 and another project having 11..this means interrupt number is not fixed to perticular HWI??? or any problem with that??