Hi all,
a customer is trying to use the AM335x clkout to drive the 32kHz clock to the WL18xx
Clock specs are from WL18xx datasheet
Accuracy: Max +/- 250ppm
Transition time: Max 100ns
Duty cycle: 15 - 85% (should be fine)
Can the AM335x output such a clock?
Thanks,
--Gunter