I have already emailed them about 20 times, first they answered me, but now they even do not answer me,Go figure!?
The Wince 7 Image on their website does not boot on my BBB, it complains about That I have a not supported BBB,
My Black bone version is A5C,
Here is the debug output, Hope somebody could help me solve the problem,
--------------------------------------------------------------------------------
Main Menu
--------------------------------------------------------------------------------
[1] Show Current Settings
[2] Select Boot Device
[3] Select KITL (Debug) Device
[4] Network Settings
[5] SDCard Settings
[6] Set Device ID
[7] Save Settings
[9] Enable/Disable OAL Retail Messages
[a] Select Display Resolution
[b] Select OPP Mode
[0] Exit and Continue
Selection: 2
--------------------------------------------------------------------------------
Select Boot Device
--------------------------------------------------------------------------------
[1] Internal EMAC
[2] NK from SDCard FILE
[0] Exit and Continue
Selection (actual Internal EMAC): 2
Boot device set to NK from SDCard FILE
--------------------------------------------------------------------------------
Main Menu
--------------------------------------------------------------------------------
[1] Show Current Settings
[2] Select Boot Device
[3] Select KITL (Debug) Device
[4] Network Settings
[5] SDCard Settings
[6] Set Device ID
[7] Save Settings
[9] Enable/Disable OAL Retail Messages
[a] Select Display Resolution
[b] Select OPP Mode
[0] Exit and Continue
Selection: 0
OEMPreDownload: Filename nk.bin
BL_IMAGE_TYPE_BIN
+OEMMultiBinNotify(0x8feb2318 -> 1)
Download file information:
-----------------------------------------------------------
[0]: Address=0x80002000 Length=0x03960d10 Save=0x80002000
-----------------------------------------------------------
Download file type: 1
+OEMIsFlashAddr(0x80002000) g_eboot.type 1
................................................................................................................................................................................................................................................................................................rom_offset=0x0.
..ImageStart = 0x80002000, ImageLength = 0x3960d10, LaunchAddr = 0x8000b940
Completed file(s):
-------------------------------------------------------------------------------
+OEMIsFlashAddr(0x80002000) g_eboot.type 1
[0]: Address=0x80002000 Length=0x3960d10 Name="" Target=RAM
ROMHDR at Address 80002044h
Launch Windows CE image by jumping to 0x8000b940...
Windows CE Kernel for ARM (Thumb Enabled)
CPU CP15 Control Register = 0xc5387f
CPU CP15 Auxiliary Control Register = 0x42
Unrecognized BeagleBoneBlack Version !
Board Name: A335BNLT
Board Ver : 0A5C
Board Ser : 3513BBBK0361
Board Type: ÿÿÿÿÿÿ
+OALTimerInit(1, 24000, 200)
--- High Performance Frequecy is 24 MHz---
I just wanted to evaluate the windows,and see what it has to offer?