This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

custom am3354 board usb enable, ti81xx driver doesn't work

Other Parts Discussed in Thread: AM3354

Hi,

I have a custom board (AM3354) loosely based on the am335x EVM. My version of u-boot is 2013.01 of the ti-sdk (psp06.00.00.00) and I'm using the linux distro from the TI board port labs ( kernel 3.2 ).

I managed to boot it and got the lcd working, with the wrong colours but we are still working on that issue.

We are now focussing on getting the usb working. Our board doesn't seem to detect any usb connected to it, and i'm positive our board is declared host.

I tried loading the drivers as module :

root@am335x-evm:/lib/modules/3.2.0-g2b92769-dirty/kernel/drivers/usb/musb# lsmod
Module                  Size  Used by
cppi41dma              25470  0
musb_hdrc              82793  1 cppi41dma
nop_usb_xceiv           1650  0
udc_core                4944  1 musb_hdrc

But when i try to load the TI81xx module i get the following message:

root@am335x-evm:/lib/modules/3.2.0-g2b92769-dirty/kernel/drivers/usb/musb# insmod ti81xx.ko
Error: could not insert module ti81xx.ko: No such device

I'm at a loss as to what the problem could be.

Our colleague thinks we have the wrong core driver and suggested we tried the usb drivers of the beaglebone.

thanks in advance