This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IPNC 4.0 Filesystem login failed ( can't execute "/sbin/getty" )

Hi,

we are trying to use the ipnc4.0's filesystem using CRAMFS not UBIFS.

I just downloaded it and make cramps without any modifications. but I can't log in to filesystem 

When I use earlier version of filesystem ( < ipnc4.0 ), it works correctly.. 

What I have to modify in IPNC4.0's filesystem?

Thanks in advance.

The follows are kernel print

[    2.946294] VFP support v0.3: not present
[    2.956125] RAMDISK: cramfs filesystem found at block 0
[    2.970348] RAMDISK: Loading 15820KiB [1 disk] into ram disk... /
[    3.922713] davinci_musb_interrupt 351: VBUS error workaround (delay coming)
[    3.930944] done.
[    4.706986] VFS: Mounted root (cramfs filesystem) readonly on device 1:0.
[    4.713929] VFS: mounted rootfs
[    4.717249] Freeing init memory: 148K
INIT: version 2.86 booting
mount: mounting /dev/mtdblock4 on /mnt/nand failed: No such device
Starting mounting local filesystems: mount mount: mounting /dev/root on / failed: No such file or directory
 failed (1: ).
/opt/ipnc/autorun.sh: line 2: /usr/sbin/avahi-autoipd: not found
/opt/ipnc/autorun.sh: line t/ipnc/autorun.sh: line 5: touch: not found
mount: mounting devpts on /dev/pts failed: No such file or directory
INIT: Entering runlevel: 5
INIT: cannot execute "/etc/init.d/rc"
INIT: cannot execute "/sbin/getty"
INIT: cannot execute "/sbin/getty"
INIT: cannot execute "/sbin/getty"
INIT: cannot execute "/sbin/getty"
INIT: cannot execute "/sbin/getty"
INIT: cannot execute "/sbin/getty"
INIT: cannot execute "/sbin/getty"
INIT: cannot execute "/sbin/getty"
INIT: cannot execute "/sbin/getty"
INIT: Id "con" respawning too fast: disabled for 5 minutes
INIT: no more processes left in this runlevel
.