This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Installing IPC on CCS V5

Hello,

I just recently downloaded CCS V5.5.00077. I read that the IPC module and its examples are installed when CCS is installed, nevertheless I dont find the package in the RTSC configurations, neither the examples.

So I downloaded the IPC modules, first the V3 (later the V1.25) and copy the extracted (from the .tar) files in /opt/ti . When I open the CCS it detect IPC automatically and add it to the RTSC configuration. But I cannot open IPC examples from templates (which is what need now), and I cannot use the ipc.h header because it doesn't work when I try to link the .obj files, from the compilation process.

I need to open the message_multicore project from the templates ( according to the C6678 simulator ) but I tried many things, even create a new template with the example but nothing has work for me until now.

Please I need help in the right procedures, to install the CCS with the IPC package or either installing the IPC after the CCS installation.

Regards,

Ronny