Hello,
I am interfacing DM365 with TM035KDH03 (LCD) which need an input Clock Frequency (Vclk) of 6.25 Mhz.
I need to generate an output clock of frequency of 6.25Mhz on VCLK(B18,GIO79) of DM365.
The external Crystal Clock Frequency i am using for the processor is 24MHz.
If I load '0x03' to DCLKCTL and DCLKPTN0 , i am getting clock frequency of 6.75 Mhz.
So Can you Pls help me to set the VCLK to 6.25 MHz?
Best Regards
Nizar