hello every one,
I want to use the example codes of ipipe given with MV5 , psp.
The problem is , I am not able to get make the project files.
the error with the header files added from LSP.Compiler is not ablr to et hte path of the header files.
Comment into the c file is,
/*kernel header file, prefix path comes from makefile */
Can any body help how can I add the prefix path ...(kernel DIRS )??????????????