Other Parts Discussed in Thread: AM3892
TI guys please help us. DM816x_AM389x_PSP_Flashing_Tools_Guide.pdf => see page 4-5: Ensure that the image (e.g. u-boot.noxip.bin) to be flashed is present in the Windows XP Machine • Load nand-flash-writer.out and run it ("Run -> Load -> Load Program" Navigate to "nand-flash-writer.out" file, open it and then run it). nand-flash-writer.out should be available in the release package Start the application from Run -> Resume. Or hit F8 • Select option 1 when prompted. Select option 2 only in case if you want to erase the whole NAND Choose your operation Enter 1 ---> To Flash an Image Enter 2 ---> To ERASE the whole NAND which path to be used for u-boot.noxip.bin, where it is located in CCS5.2 where is the option 1 prompt, in debugger or serial terminal regards vivek