hi all.when i set all the enc dynamic parameters at the same time over some range,it will be segment fault.
for example
RcAlg=0(VBR)
Resolution=(1920*1080)
encIntraFrameInterval = 500;
FrameRate = 60
BitRate = 40000
qpMin = 20;
qpMax = 52
BUT I JUST change the Resolution to 352*288 ,it will not have segment fault .
alse i change the BitRate = 50000,encIntraFrameInterval =200,it will alse have segment fault.
if i just change one parameters at run time,i will have the following errors,but app is still running and not down
Enter Choice: [m3video] 60530:!ERROR!:ENCLINK::links_m3video/iva_enc/encLink_h264.c:[232]::INTERNAL ERROR:-1
[m3video] ALGCONTROL FAILED:CMD:1
[m3video] ERROR: IH264ENC_LEVEL_INCOMPLAINT_PARAMETER , 0,
[m3video] 60531:WARN
[m3video] ENCLINK: ERROR in Run time parameters changes, Extended Error code:1
so how should i constuct the above parameters.