This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Appro 5.1



                       We are currently developing a Digital Video Encoder based on DM365 and using Appro 5.1 SDK. We have modified the Appro 5.1 SDK u-boot and kernel. Following are the changes done:
1. In u-boot added support for ethernet PHY(RTL8201)
2. In kernel changed NAND partion.NAND partition used is:
        0x000000000000-0x000000200000 : "bootloader"
        0x000000200000-0x000000400000 : "params"
        0x000000400000-0x000000900000 : "kernel"
        0x000000900000-0x000002900000 : "filesystem"
        0x000002900000-0x000003000000 : "config"
        0x000003000000-0x000003500000 : "kernel_recovery"
        0x000003500000-0x000004500000 : "filesystem_recovery"
        0x000004500000-0x000004f00000 : "syslog"

Details of NAND flash used:
        Part number - K9F1G08X0C
        Page size-2KB
        Block size-128KB
        Spare area - 4K

3. UBIFS filesystem is created using commands:
           mkfs.ubifs -r  filesys_dm365 -m 2048 -e 126976 -c 313 -o ubifs.img
           ubinize -o ipnc_dm365_ubifs -m 2048 -p 128KiB  dm365_ubinize.cfg
                 
4.Bootargs used is:
                setenv 256mbootargs 'set bootargs mem=45M console=ttyS0,115200n8 ip=off rw ubi.mtd=3,2048     rootfstype=ubifs root=ubi0:rootfs cmemk.phys_start=0x82d00000 cmemk.phys_end=0x87f00000  cmemk.phys_start_1=0x00001000 cmemk.phys_end_1=0x00008000 cmemk.pools_1=1x28672 cmemk.allowOverlap=1 cmemk.useHeapIfPoolUnavailable=1 nohz=off highres=off clocksource=acpi_pm lpj=739328 eth=$(ethaddr)'

               We have successfully compiled the u-boot, kernel and UBIFS filesystem. When trying to do NAND boot after flashing the kernel and filesystem(flashing is done after giving "nand scrub") getting following issues:

1. following blocks are shown as bad blocks:
        0x000000400000 - 0x0000007e0000
        0x000002140000 - 0x0000023e0000
2. Getting errors:
        UBI error: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB 0:0, read 64 bytes
        UBI error: ubi_io_read: error -74 (ECC error) while reading 512 bytes from PEB 0:2048, read 512 bytes
        VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0)
        [    6.030715] Please append a correct "root=" boot option; here are the available partitions:
        [    6.039151] 1f00            2048 mtdblock0  (driver?)
        [    6.044404] 1f01            2048 mtdblock1  (driver?)
        [    6.049514] 1f02            5120 mtdblock2  (driver?)
        [    6.054724] 1f03           32768 mtdblock3  (driver?)
        [    6.059833] 1f04            7168 mtdblock4  (driver?)
        [    6.065025] 1f05            5120 mtdblock5  (driver?)
        [    6.070196] 1f06           16384 mtdblock6  (driver?)
        [    6.075307] 1f07           10240 mtdblock7  (driver?)
        [    6.080471] 1f08           50176 mtdblock8  (driver?)
        [    6.085574] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
        [    6.093923] Backtrace:
        [    6.096412] Function entered at [<c002e4ec>] from [<c033475c>]
        [    6.102321]  r7:00008000 r6:c2813000 r5:c00238f0 r4:c03dea60
        [    6.108062] Function entered at [<c0334744>] from [<c03347c8>]
        [    6.113969] Function entered at [<c0334760>] from [<c0008fc0>]
        [    6.119829]  r3:00000000 r2:00000000 r1:c2825f78 r0:c0355a9e
        [    6.125619] Function entered at [<c0008ddc>] from [<c000916c>]
        [    6.131528] Function entered at [<c00090d8>] from [<c00084b4>]
        [    6.137389]  r5:c002308c r4:c03de298
        [    6.141062] Function entered at [<c00083a4>] from [<c0042e78>]
        [    6.146919]  r5:c00083a4 r4:00000000

                                We are able to boot with NFS but "bad block" issue is present.

         Any help will be appreciated.
         

   

  • Hi,

    1. following blocks are shown as bad blocks:
            0x000000400000 - 0x0000007e0000
            0x000002140000 - 0x0000023e0000


    If you want to check those blocks are really bad,  you can see all bad blocks get skipped/listed during nand srcub as you said

    0x400000 ---> this location is kernel area

    it could be mismatch ECC types between bootloader & kernel

    Try to change the ECC type in board file   

    ".ecc_mode        = NAND_ECC_HW,"

       .ecc_mode        = NAND_ECC_SW,

       .ecc_mode        = NAND_ECC_HW_SYNDROME,

    use anyone of this & flash kernel with these modification compiled image

    Which ECC type are you using?


    UBIFS

    -----------


    Refer the below links for UBIFS suport

    http://processors.wiki.ti.com/index.php/UBIFS_Support
    http://elinux.org/UBIFS
    http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3.4-DevKit-2.1_UserGuide#Fastboot_and_UBI_rootfs


               mkfs.ubifs -r  filesys_dm365 -m 2048 -e 126976 -c 313 -o ubifs.img

    For 32MB fs storage , 313 is it OK?

    See

    Boot your s/m in NFS mode , flash the filesystem with UBIFS type then try to mount the partition (for testing) then go for initial UBIFS mounting (through bootargs and all)

    In target shell (NFS boot)

    -------------------------------------

    # flash_eraseall /dev/mtd3

    # ubiformat /dev/mtd3 -s 512 -y   (

    # ubiattach /dev/ubi_ctrl -m 3

    # mount -t ubifs ubi0:ubi-rootfs /mnt/

    make any changes as you want

    # umount /mnt

    # ubidetach /dev/ubi_ctrl -m 3



    Regards,

    Titus S.

    Refer the below link for UBIFS suport

  • Hi,
           Thank's for your reply.

             Checked ECC in u-boot and kernel, earlier "NAND_ECC_HW_SYNDROME" was set in u-boot and "NAND_ECC_HW" in kernel. For UBIFS the value used for argument -c(313) was wrong. Calculated this value and got 250.

     Tried by setting same ECC in u-boot and kernel and following is the result:

    NAND_ECC_HW:
         Getting bad block issue

    NAND_ECC_SW:
         Showing bad blocks at 02900000 - 02fe0000(This area is after the filesystem partition)
         We are able to Load UBIFS if programmed from linux,following are the steps done:
             -Done NFS boot
         -Erased filesystem partition using command "flash_eraseall /dev/mtd3"
         -Flashed filesystem using command "flashcp filesystem_image /dev/mtd3"
             -Then tried to do NAND boot with bootargs.
       But not able to load UBIFS if programmed from u-boot.

    NAND_ECC_HW_SYNDROME:
         NAND driver probe failed - "davinci_nand: probe of davinci_nand.0 failed with error -22"

    Regards,
       Geethu
         
        



         
        

  • Hi,

    NAND BAD BLCOK

    You can use "NAND_ECC_HW" type ECC

    I think, you are using wrong SDK's (may be your using new SDK's kernel with old SDK's uboot) (mismatch versions)

    i faced the same kind of issue when i try to use new kernel with old uboot binary.

    UBIFS

    We are able to Load UBIFS if programmed from linux,following are the steps done:
             -Done NFS boot
         -Erased filesystem partition using command "flash_eraseall /dev/mtd3"
         -Flashed filesystem using command "flashcp filesystem_image /dev/mtd3"


    Can you able to list/check the filesystem, which you have written while you are in NFS mode?

    do the below commands after NFS boot (copy rootfs.ubi file into NFS fs)

    flash_eraseall /dev/mtd3

    ubiformat /dev/mtd3 -f rootfs.ubi -O 512  (chk it)

    ubiattach /dev/ubi_ctrl -m 3

    mount -t ubifs ubi0 /mnt

    ls /mnt          (check here ; all files are avail?)

    >> If you able to see properly(without any errors) then only u can able to mount initial time(thr bootargs)

    umount /mnt

    ubidetach /dev/ubi_ctrl -m 3

    NOTE

    Do you have any intended reason to boot with ubifs & why not yaffs2?

    yaffs2 is much easier than ubifs (steps)




  • Hi,

    Can you please provide complete bootup log (top to bottom) start with bootloader upto error.

    You can list actual bad blocks list at uboot section by "nand bad" command & paste that too

    Are you getting any error while you are doing "saveenv"?

    What SDK version are you using?

  • Hi,

    Refer my old post,

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/p/204957/727450.aspx#727450

    I got fixed this by doing the below things,

    Have a try,

    Scenario (How i hv faced this issue on my custom board?)

    ==============================================

    In my custom board, very first time i have flashed 2.6.18 kernel (LSP2.10) & with the same old LSP2.10's u-boot

    after that i flashed new u-boot & kernel (LSP3.10 of TI), then i got the bad block errors,

    This is because of due to bbt (bad block table) of  old with new one(type of ECC)

    Fix

    ===

    I have used new PSP3.10's kernel image & u-boot,

    1) flashed ubl (old) & , u-boot(old)

    2) nand scrub

    3) flash new UBL, u-boot & kernel

    fixed !!!

  • Hi,

    Bad blocks listed after NAND scrub:
    ===========================================================================
     03960000
     052a0000
     07760000
     077c0000
     07f80000
     07fa0000
     07fc0000
     07fe0000

    Bad blocks listed after flashing Kernel,filesystem and doing NAND boot :
    ===========================================================================
      00200000
      00400000
      00420000
      00440000
      00460000
      00480000
      004a0000
      004c0000
      004e0000
      00500000
      00520000
      00540000
      00560000
      00580000
      005a0000
      005c0000
      005e0000
      00600000
      00620000
      00640000
      00660000
      00680000
      006a0000
      006c0000
      006e0000
      00700000
      00720000
      00740000
      00760000
      00780000
      007e0000
      02160000
      02180000
      021a0000
      021c0000
      021e0000
      02200000
      02220000
      02240000
      02260000
      02280000
      022a0000
      022c0000
      022e0000
      02300000
      02320000
      02340000
      02360000
      02380000
      023a0000
      023c0000
      023e0000
      03960000
      052a0000
      07760000
      077c0000
      07f80000
      07fa0000
      07fc0000
      07fe0000

         After getting these bad blocks if we give saveenv getting error:
                     Saving Environment to NAND...
             Erasing Nand...
             Skipping bad block at  0x00200000                                            
             Writing to Nand... FAILED!

        We are using SDK5.1
        Please find the attached logs.

    Regards,
       Geethu

    7041.log.txt

  • Hi,

      I tried the fix you suggested :

          1) flashed ubl (old) & , u-boot(old)

          2) nand scrub

          3) flash new UBL, u-boot & kernel

    But getting the same issue.

    Regards,

        Geethu

  • Hi,

    How you are flashing the UBL & U-boot? (SD card or nandwriter or serial flasher)

    Can you try to flash to your ubl & u-boot bn through serial flasher utility?

    Please provide NAND Part no?

    Refer the below link & verfiy the NAND ECC layout in your ubl & u-boot code

    http://processors.wiki.ti.com/index.php/DM365_Nand_ECC_layout

    Do you have any command like "nand ecc hw" in u-boot terminal?


    Try to boot the board from ramdisk & flash kernel image and filesystem into NAND flash through mtd-utils (ie flashing kernel & fs with ECC layout of linux)
    It seems to be issue with ECC layout of u-boot.

    Is this your custom board or TI EVM?
    if it is custom, Aru using same nand flash in your board as EVM?

  • Hi,

    Try to flash kernel image & fs by linux ECC type (from linux shell)

    do the below commands after NFS boot (copy rootfs.ubi file & kernel into NFS fs)

    Kernel

    =======

    copy the kernel image into NFS fs folder

    $ flash_eraseall /dev/mtd2  (kernel partition)

    $ nandwrite -p /dev/mtd2 /uImage_ipnc_dm365 (flashing kernel at 0x400000 to 0x900000)


    Filesystem

    ==========

    flash_eraseall /dev/mtd3

    ubiformat /dev/mtd3 -f rootfs.ubi -O 512  (chk it)

    ubiattach /dev/ubi_ctrl -m 3

    mount -t ubifs ubi0 /mnt

    ls /mnt          (check here ; all files are avail?)

    >> If you able to see properly(without any errors) then only u can able to mount initial time(thr bootargs)

    umount /mnt

    ubidetach /dev/ubi_ctrl -m 3

  • Hi,

        Thank's for your replay.

        We will try these suggestions.

    Regards,

       Geethu

  • Hi

    We are using kernel 2.6.32 and we are facing following error on TI  DM355 Evm


    Our NAND is spansion S34ML08G1.

    our nand ECC bit is 1

    uncorrectable error :

    Please reply me as soon as possible

  • Hi Tejas Dave,

    Did you resolve the issue you were chasing?

    Setup: DM368 based IP camera.

    I'm chasing something somewhat related.  I have about 30k devices deployed.  We're rolling out a new build of firmware.  What I've found is that the flash_eraseall on the yaffs2 partition occasionally fails or leaves the device in an incomplete state.  After the erase no files are able to be written to the partition until a hard power cycle occurs.

    This causes a portion of our upgrades to fail the upgrade process... and in this case dumps us back out to UBOOT.... which is unacceptable....

    Could this possibly be explained by kernel settings:

    board-dm365-evm.c: ~333

    static struct nand_davinci_platform_data nand_data = {
     .options = 0,
     .ecc_mode = NAND_ECC_HW_SYNDROME,   /* Reed-Solomon with inline syndrome */
     /* .ecc_mode = NAND_ECC_SOFT, */
     /* .ecc_mode = NAND_ECC_HW, */

     

    or perhaps using an old UBOOT version?

    We're currently still using our original UBOOT build from ~2009.  We had updated the UBL to fix a soft boot hang problem.. but hadn't yet been motivated to upgrade the UBOOT...

    Regards,

    Edwin